LPUART pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPUART pins

跳至解决方案
3,482 次查看
sapirbuz
Contributor IV

Hi,

Can LPUART3 work using the following pins?

LPUART3_TXD- GPIO_B0_08

LPUART3_RXD- GPIO_EMC_14

LPUART3_CTS_B- GPIO_AD_B1_04

LPUART3_RTS_B- GPIO_EMC_16

In case yes, what will happen when the EMC bank is 1.8v and the GPIO bank is 3.3V?






0 项奖励
回复
1 解答
3,454 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you. Those pins have LPUART functionality and can be used.  Please consider that powering the rails with different voltages will have different output voltages in each pin.

Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,471 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
Could you please provide me the part number you are using? This to confirm  if LPUART3 is present on those pins.

If EMC bank is 1.8v, the output from those pins will be 1.8v while the GPIO_AD bank output will be 3.3v. This could cause issues depending on the operating voltage of the device you´re trying to communicate.

Best regards,
Omar

0 项奖励
回复
3,460 次查看
sapirbuz
Contributor IV

thank you

the PN is MIMXRT1051CVL5B

0 项奖励
回复
3,455 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you. Those pins have LPUART functionality and can be used.  Please consider that powering the rails with different voltages will have different output voltages in each pin.

Best regards,
Omar

0 项奖励
回复
3,444 次查看
sapirbuz
Contributor IV

thank you

0 项奖励
回复