Imx6dl with 16bit DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6dl with 16bit DDR3

619 Views
adrian_dusinski
Contributor II

adrian_dusinski_0-1653928871293.png

Regarding the image above Imx6dl support only 32 and 64 bit DDR3 but is it completely impossible to use 16 bit DDR?

Regards,

Adrian

 

Labels (1)
0 Kudos
Reply
2 Replies

596 Views
adrian_dusinski
Contributor II

Thanks for reponse.

0 Kudos
Reply

611 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the data sheet:

External memory interfaces: The i.MX 6Solo/6DualLite processors support latest, high volume,
cost effective handheld DRAM, NOR, and NAND Flash memory standards.
— 16/32-bit LP-DDR2-800, 16/32-bit DDR3-800 and DDR3L-800 in i.MX 6Solo; 16/32/64-bit
LP-DDR2-800, 16/32/64-bit DDR3-800 and DDR3L-800, supporting DDR interleaving mode
for 2x32 LPDDR2-800 in i.MX 6DualLite

 

0 Kudos
Reply