LPDDR4 part selection for i.MX8 DualXPlus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPDDR4 part selection for i.MX8 DualXPlus

1,329 次查看
kailas_kharse
Contributor IV

Hello Team,

We going to design our custom board using iMXDualXPlus.

As there is Micron's LPDDR4 used on EVK board. We have plan to use JEDEC-compliant LPDDR4 8Gb (x16 x 2 channel ) provided by the customer for custom board?

Is there any known issue or risk if I use this part?

 
Please provide a solution to this topic as soon as possible because I require it's solution very urgent.

Which i.MX family DDR Tools I can use for i.Mx8DualXPlus?

What are the modifications we need to do in U-Boot OR Kernel for using different LPDDR4 Memory?

Regards,

Kailas Kharse

0 项奖励
回复
2 回复数

1,236 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kailas

I believe this part can be used with i.MX8 DualXPlus.

>Which i.MX family DDR Tools I can use for i.Mx8DualXPlus?

i.MX 8/8X Family DDR Tools Release  

>What are the modifications we need to do in U-Boot OR Kernel for using different LPDDR4 Memory?

please follow guidelines given in MX8X_DDR_Tools_quickstart_guide.pdf on that link.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,236 次查看
kailas_kharse
Contributor IV

Hello Igor,

I have one more Use Case, I want to use Octal RAM which is interfaced via Flex SPI.

So is it possible to use Octal RAM instead of LPDDR4?

What are the changes need to use Octal RAM instead of LPDDR4 for I.Mx8DualxPlus Processor?

Thanks,

Kailas Kharse

0 项奖励
回复