LPDDR2 support on imx6sll

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR2 support on imx6sll

1,719 Views
buy
Contributor I

Hi,

The iMX6SLL Data Sheet (https://www.nxp.com/docs/en/data-sheet/IMX6SLLCEC.pdf) clearly states, that iMX6SLL supports BOTH LPDDR2 and LPDDR3. We have bought a huge branch of iMX6SLL (MCIMX6V7DVN10AB) to use in our Yocto project.

However, now I cannot find the full support of LPDDR2 in BSP. In particular, for the deep sleep.

Could somebody clarify the situation?

Thanks

Labels (3)
Tags (2)
1 Reply

1,614 Views
igorpadykov
NXP Employee
NXP Employee

Hi dR

seems one can reuse i.MX6SL EVK software (lpddr2 based design) as

i.MX6SLL is pin-to-pin compatible with i.MX6SL, according to AN11988

"i.MX6SLL Migration Guide, Migrating from i.MX6SL to i.MX6SLL "

https://www.nxp.com/docs/en/application-note/AN11988.pdf 

also one can look on linux/arch/arm/boot/dts/imx6sll-lpddr2-arm2.dts

imx6sll-lpddr2-arm2.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

linux/arch/arm/mach-imx/suspend-imx6.S

suspend-imx6.S\mach-imx\arm\arch - linux-imx - i.MX Linux kernel 

Linux documentation (Linux Manual, "Low Level Power Management (PM)")

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply