LCD display Flickering

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LCD display Flickering

1,133 次查看
kishorepoojari
Contributor III

Hello All,

   We are using imx233 processor and LCD display with the spec:

Resolution:320*240

Bus width:16bit

pixel clock:6MHz

   LCD Display will start to flicker when control is transferred  from bootloader to O.S , where frame buffer starting address will be changed .  Please let me known is their any solution to over come this problem.

Regards,

Kishore P

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

942 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kishore

one can try approach described on

Patch to support uboot logo keep from uboot to kernel to Android for JB4.2.2_1.1.0-GA and L3.0.35_4....

though I am not aware of similar patch for i.MX23.

Other option move lcd initialization to kernel phase, making bootloader as short as

possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复