LCD display Flickering

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD display Flickering

1,705 Views
kishorepoojari
Contributor III

Hello All,

   We are using imx233 processor and LCD display with the spec:

Resolution:320*240

Bus width:16bit

pixel clock:6MHz

   LCD Display will start to flicker when control is transferred  from bootloader to O.S , where frame buffer starting address will be changed .  Please let me known is their any solution to over come this problem.

Regards,

Kishore P

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,514 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kishore

one can try approach described on

Patch to support uboot logo keep from uboot to kernel to Android for JB4.2.2_1.1.0-GA and L3.0.35_4....

though I am not aware of similar patch for i.MX23.

Other option move lcd initialization to kernel phase, making bootloader as short as

possible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply