LCD & Camera Module for IMX6ULLEVKHUG Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD & Camera Module for IMX6ULLEVKHUG Board

1,463 Views
Embedded-world
Contributor IV

Dear Experts.

For the IMX6ULLEVKHUG Board, which LCD and camera module are suitable? Could someone kindly share some datasheets for both modules?


Thank you & Regards,

Ravikumar

0 Kudos
Reply
2 Replies

1,431 Views
Embedded-world
Contributor IV

Hi @Chavira 

Thank you for the information. If you could provide a reference link (Part Number) for an LCD module tested with i.MX6ULL, that would be even more useful for me.


Thank you & Regards, 
Ravikumar.

0 Kudos
Reply

1,442 Views
Chavira
NXP TechSupport
NXP TechSupport
 
We don't have the part number for cusotmers. Because many LCD modules can be used on i.MX6ULL processor.
 
BUT my suggestion is that you can contact a LCD provider, and ask him to
selcet a type of LCD module, your requirments can be like this:
1. RGB666 parallel interface.
2. 800x600 , or 640x480 resolution
 
The camera for iMX6ULL can be the next: