LCD Screen Selection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD Screen Selection

2,398 Views
oferlivny
Contributor I

Hi

I'm starting to develop on MX6 ARM2 CPU board, and I'm looking for the easiest solution for connecting a screen to the board.

I'm working with embedded linux, and don't have any specific requirements from the screen (other than it being small - 10 inch or so, and quick and easy setup). I need it mainly to for debug (other than using a terminal).

Did anyone had a good experience with integrating a display with this board through quick and easy setup and can post its details here?

Labels (1)
0 Kudos
Reply
3 Replies

2,318 Views
PrabhuSundarara
NXP Employee
NXP Employee

LVDS

http://www.hannstar.com/Common.aspx?mid=198&tmid=3&modid=4

 

BSP already has support for these displays. No need of any extra effort for integrating these displays.

0 Kudos
Reply

2,318 Views
oferlivny
Contributor I

Thanks for the reply!

Can you please specify a specific model of a display you have experienced with?

Will all displays require the same integration effort?



Prabhu Sundararaj said:

Easiest is using HDMI or LVDS display. If your requirement is limited to use 10 inch display, then go for LVDS display.

0 Kudos
Reply

2,318 Views
PrabhuSundarara
NXP Employee
NXP Employee

Easiest is using HDMI or LVDS display. If your requirement is limited to use 10 inch display, then go for LVDS display.

0 Kudos
Reply