LCD Screen Selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD Screen Selection

2,409件の閲覧回数
oferlivny
Contributor I

Hi

I'm starting to develop on MX6 ARM2 CPU board, and I'm looking for the easiest solution for connecting a screen to the board.

I'm working with embedded linux, and don't have any specific requirements from the screen (other than it being small - 10 inch or so, and quick and easy setup). I need it mainly to for debug (other than using a terminal).

Did anyone had a good experience with integrating a display with this board through quick and easy setup and can post its details here?

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,329件の閲覧回数
PrabhuSundarara
NXP Employee
NXP Employee

LVDS

http://www.hannstar.com/Common.aspx?mid=198&tmid=3&modid=4

 

BSP already has support for these displays. No need of any extra effort for integrating these displays.

0 件の賞賛
返信

2,329件の閲覧回数
oferlivny
Contributor I

Thanks for the reply!

Can you please specify a specific model of a display you have experienced with?

Will all displays require the same integration effort?



Prabhu Sundararaj said:

Easiest is using HDMI or LVDS display. If your requirement is limited to use 10 inch display, then go for LVDS display.

0 件の賞賛
返信

2,329件の閲覧回数
PrabhuSundarara
NXP Employee
NXP Employee

Easiest is using HDMI or LVDS display. If your requirement is limited to use 10 inch display, then go for LVDS display.

0 件の賞賛
返信