LCD RGB Color problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LCD RGB Color problem

1,627 次查看
deepanrajanbara
Contributor IV

Hi,

Ours is imx6q processor in which we have integrated a LVDS 800x600 display in Linux 3.10.17 with Yocto .So we have set all the parameters  according to the Datasheet .In software we have configured all the parameters in linux/drivers/video/mxc/ldb.c and the RGB value setting and bits per pixel value have been set in linux/arch/arm/boot/dts/*.dtsi file.But image obtained was not proper and there is some RGB mismatch. Can any one please conform what could be the mistake when configuring the LVDS with 6-bit RGB each.

Thank you,

Deepanraj.A

0 项奖励
回复
1 回复

1,428 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Deepanraj,

On the following thread’s responses you could find useful information regarding LCDs configurations on 640x480 resolution on i.MX processors:

Configuring the resolution of the VGA to support 800x600 and 640x480

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复