Hi all,
In my customer board which is iMX6SL based with 18-bit is required.
But I can not find the description of mapping of LCD_D[0..17] to RGB components in RM. Help is need, thanks in advance.
Ko-hey
解決済! 解決策の投稿を見る。
Hi Ko-key,
About the 8bit/16bit/18bit/24bit use you can see the detail use in 20.4.12 LCDIF Pin Usage by Interface Mode in the i.MX6SL RM.
Take the the 18bit RGB666 as an example:
(1) RED
LCD_DATA12~LCD_DATA17
(2) GREEN
LCD_DATA06~LCD_DATA11
(3) BLUE
LCD_DATA00~LCD_DATA05
Have a great day,
Rita
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Could someone answer and follow this question ?
Ko-hey
Hi Ko-key,
About the 8bit/16bit/18bit/24bit use you can see the detail use in 20.4.12 LCDIF Pin Usage by Interface Mode in the i.MX6SL RM.
Take the the 18bit RGB666 as an example:
(1) RED
LCD_DATA12~LCD_DATA17
(2) GREEN
LCD_DATA06~LCD_DATA11
(3) BLUE
LCD_DATA00~LCD_DATA05
Have a great day,
Rita
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi b45499
Let me confirm the connection again.
Are the following connections correct ?
LCD_DATA00~LCD_DATA05:B0~B5
LCD_DATA06~LCD_DATA11:G0~G5
LCD_DATA12~LCD_DATA17:R0~R5
Ko-hey
Hi Ko-hey,
Can you send you LCD screen datasheet or LCD interface information to us? The connection also depend on the screen you are using.
Have a great day,
Rita
Hi Rita Wang
I made a Case 00221192 because it is confidential infromation.
Could you check the case ?
Ko-hey
Hi Ko-hey,
I have confirmed it for you that your connection is right.
Have a nice day
Rita
Hi Ko-key,
I am confirming it for you, and then give you reply as soon as possible.
Have a nice day
Rita