LCD_DATAx RGB mapping for i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD_DATAx RGB mapping for i.MX6SL

Jump to solution
2,868 Views
ko-hey
Senior Contributor II

Hi all,

 

In my customer board which is iMX6SL based with 18-bit is required.

But I can not find the description of mapping of LCD_D[0..17] to RGB components in RM. Help is need, thanks in advance.

 

Ko-hey

 

0 Kudos
Reply
1 Solution
2,703 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ko-key,

About the 8bit/16bit/18bit/24bit use you can see the detail use in 20.4.12 LCDIF Pin Usage by Interface Mode in the i.MX6SL RM.

Take the the 18bit RGB666 as an example:

(1) RED
LCD_DATA12~LCD_DATA17
(2) GREEN
LCD_DATA06~LCD_DATA11
(3) BLUE
LCD_DATA00~LCD_DATA05
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
7 Replies
2,703 Views
ko-hey
Senior Contributor II

Could someone answer and follow this question ?

Ko-hey

0 Kudos
Reply
2,704 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ko-key,

About the 8bit/16bit/18bit/24bit use you can see the detail use in 20.4.12 LCDIF Pin Usage by Interface Mode in the i.MX6SL RM.

Take the the 18bit RGB666 as an example:

(1) RED
LCD_DATA12~LCD_DATA17
(2) GREEN
LCD_DATA06~LCD_DATA11
(3) BLUE
LCD_DATA00~LCD_DATA05
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,703 Views
ko-hey
Senior Contributor II

Hi b45499

Let me confirm the connection again.

Are the following connections correct ?

LCD_DATA00~LCD_DATA05B0B5

LCD_DATA06~LCD_DATA11G0G5

LCD_DATA12~LCD_DATA17R0R5

Ko-hey

0 Kudos
Reply
2,703 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ko-hey,

Can you send you LCD screen datasheet or LCD interface information to us? The connection also depend on the screen you are using.

Have a great day,
Rita

0 Kudos
Reply
2,703 Views
ko-hey
Senior Contributor II

Hi Rita Wang

I made a Case 00221192 because it is confidential infromation.

Could you check the case ?

Ko-hey

0 Kudos
Reply
2,703 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ko-hey,

I have confirmed it for you that your connection is right.

Have a nice day

Rita

2,703 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ko-key,

I am confirming it for you, and then give you reply as soon as possible.

Have a nice day

Rita

0 Kudos
Reply