[L5.10.72_2.2.0_i.MX_Desktop_POC_GA] Add opencv-imx into Ubuntu based rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[L5.10.72_2.2.0_i.MX_Desktop_POC_GA] Add opencv-imx into Ubuntu based rootfs

1,013 Views
khang_letruong
Senior Contributor III

Dear Community,

I would like to know if it is possible to add opencv-imx (libraries and headers) into the rootfs of Ubuntu based firmware image during the compilation with Yocto, please ?

Thanks in advance and best regards,
Khang

0 Kudos
Reply
3 Replies

943 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The OpenCV is optimized for machine learning in the eIQ of the i.MX family and the documentation is the same. For example you can see the The Linux User Guide, in your yocto documents.

https://source.codeaurora.org/external/imx/opencv-imx/?h=github.com%2F5.x

https://github.com/opencv/opencv

0 Kudos
Reply

984 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using?

0 Kudos
Reply

981 Views
khang_letruong
Senior Contributor III

Hi @Rita_Wang ,

I am using IMX8MP EVK.

0 Kudos
Reply