[L5.10.72_2.2.0_i.MX_Desktop_POC_GA] Add opencv-imx into Ubuntu based rootfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[L5.10.72_2.2.0_i.MX_Desktop_POC_GA] Add opencv-imx into Ubuntu based rootfs

1,082 次查看
khang_letruong
Senior Contributor III

Dear Community,

I would like to know if it is possible to add opencv-imx (libraries and headers) into the rootfs of Ubuntu based firmware image during the compilation with Yocto, please ?

Thanks in advance and best regards,
Khang

0 项奖励
回复
3 回复数

1,012 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The OpenCV is optimized for machine learning in the eIQ of the i.MX family and the documentation is the same. For example you can see the The Linux User Guide, in your yocto documents.

https://source.codeaurora.org/external/imx/opencv-imx/?h=github.com%2F5.x

https://github.com/opencv/opencv

0 项奖励
回复

1,053 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using?

0 项奖励
回复

1,050 次查看
khang_letruong
Senior Contributor III

Hi @Rita_Wang ,

I am using IMX8MP EVK.

0 项奖励
回复