[L5.10.72_2.2.0_i.MX_Desktop_POC_GA] Add opencv-imx into Ubuntu based rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[L5.10.72_2.2.0_i.MX_Desktop_POC_GA] Add opencv-imx into Ubuntu based rootfs

1,017件の閲覧回数
khang_letruong
Senior Contributor III

Dear Community,

I would like to know if it is possible to add opencv-imx (libraries and headers) into the rootfs of Ubuntu based firmware image during the compilation with Yocto, please ?

Thanks in advance and best regards,
Khang

0 件の賞賛
返信
3 返答(返信)

947件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The OpenCV is optimized for machine learning in the eIQ of the i.MX family and the documentation is the same. For example you can see the The Linux User Guide, in your yocto documents.

https://source.codeaurora.org/external/imx/opencv-imx/?h=github.com%2F5.x

https://github.com/opencv/opencv

0 件の賞賛
返信

988件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using?

0 件の賞賛
返信

985件の閲覧回数
khang_letruong
Senior Contributor III

Hi @Rita_Wang ,

I am using IMX8MP EVK.

0 件の賞賛
返信