L4.1.15-1.0.0_ga-mfg-tools support for i.MX 6ULL EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

L4.1.15-1.0.0_ga-mfg-tools support for i.MX 6ULL EVK

1,806件の閲覧回数
jayabc
Contributor I

I want to flash bsp to NAND of i.MX 6ULL EVK using Mfg tool. Could some suggest correct settings and procedure to flash NAND using mfg tool. 

Thanks in advance

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,546件の閲覧回数
jayabc
Contributor I

Thanks Joan,

But I want support for 

 

I want to flash bsp (u-boot, kenel,dtb,rootfs) to SDcard through USB-OTG using Mfg tool. I am using i.mx6ull evk board.

I have set boot mode to internal ROM. My board is detected and recognised as “HID-complaint device”. I have taken package “L4.9.11_1.0.0-ga_mfg-tools.tar” for mfg tool.

But I am not sure about what values to be set for parameters given in cfg.ini file for  i.mx6ull board. I have searched in nxp community, but no luck.

 

Could you please help me for values to be set for :

 

[profiles]

chip = Linux

 

[platform]

board = ??

 

[LIST]

name = SDCard

 

[variable]

board = ??

0 件の賞賛
返信

1,546件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

one can refer to the document as below, which is for imx6ul evk, but it's similar with imx6ull evk

https://community.nxp.com/docs/DOC-236994 

0 件の賞賛
返信

1,546件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link as belowNand Flash in IMX6ULL EVK 

if  you add  new nand flash, don't forget to add them to the nand_ids.c 

0 件の賞賛
返信