L4.1.15-1.0.0_ga-mfg-tools support for i.MX 6ULL EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

L4.1.15-1.0.0_ga-mfg-tools support for i.MX 6ULL EVK

1,807 次查看
jayabc
Contributor I

I want to flash bsp to NAND of i.MX 6ULL EVK using Mfg tool. Could some suggest correct settings and procedure to flash NAND using mfg tool. 

Thanks in advance

标签 (1)
0 项奖励
回复
3 回复数

1,547 次查看
jayabc
Contributor I

Thanks Joan,

But I want support for 

 

I want to flash bsp (u-boot, kenel,dtb,rootfs) to SDcard through USB-OTG using Mfg tool. I am using i.mx6ull evk board.

I have set boot mode to internal ROM. My board is detected and recognised as “HID-complaint device”. I have taken package “L4.9.11_1.0.0-ga_mfg-tools.tar” for mfg tool.

But I am not sure about what values to be set for parameters given in cfg.ini file for  i.mx6ull board. I have searched in nxp community, but no luck.

 

Could you please help me for values to be set for :

 

[profiles]

chip = Linux

 

[platform]

board = ??

 

[LIST]

name = SDCard

 

[variable]

board = ??

0 项奖励
回复

1,547 次查看
joanxie
NXP TechSupport
NXP TechSupport

one can refer to the document as below, which is for imx6ul evk, but it's similar with imx6ull evk

https://community.nxp.com/docs/DOC-236994 

0 项奖励
回复

1,547 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link as belowNand Flash in IMX6ULL EVK 

if  you add  new nand flash, don't forget to add them to the nand_ids.c 

0 项奖励
回复