L2 cache for MCIMX6G0DVM05AA ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

L2 cache for MCIMX6G0DVM05AA ?

ソリューションへジャンプ
2,703件の閲覧回数
CarstenBode
Contributor II

Hello together,

I´m not sure if the smallest IMX6UL has a L2 cache:

The block diagram that shows the optional block dottet indicates the presence of 128k L2C on all versions.

The datasheet only refers to the feature set Baseline/ General purpose 1 and 2 and security, no details.

The UL Fact sheet shows no L2 cache for the G0 version.

ラベル(1)
1 解決策
2,526件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carsten Bode,

As you mentioned, the L2 cache block is marked as optional in some i.MX6UL Part Numbers. The G0 version of the i.MX6UL is the less equipped of the i.MX6UL processors and indeed does not have L2 Cache so the information on the Fact Sheet is correct. If this is a requirement for your design I would recommend using the G1 version.

I hope this information helps!

元の投稿で解決策を見る

3 返答(返信)
2,527件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carsten Bode,

As you mentioned, the L2 cache block is marked as optional in some i.MX6UL Part Numbers. The G0 version of the i.MX6UL is the less equipped of the i.MX6UL processors and indeed does not have L2 Cache so the information on the Fact Sheet is correct. If this is a requirement for your design I would recommend using the G1 version.

I hope this information helps!

2,526件の閲覧回数
CarstenBode
Contributor II

Hello gusarambulo,

ok, thanks for the clarification, I understand that the L2 cache block is missing.

I assume the SCU is still present because it is separate from the L2C on the Corte A7.

Best regards

Carsten

2,526件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carsten Bide,

You are correct, the SCU is still present even if no L2 cache is available.

Regards,