L2 cache for MCIMX6G0DVM05AA ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

L2 cache for MCIMX6G0DVM05AA ?

跳至解决方案
1,708 次查看
CarstenBode
Contributor II

Hello together,

I´m not sure if the smallest IMX6UL has a L2 cache:

The block diagram that shows the optional block dottet indicates the presence of 128k L2C on all versions.

The datasheet only refers to the feature set Baseline/ General purpose 1 and 2 and security, no details.

The UL Fact sheet shows no L2 cache for the G0 version.

标签 (1)
1 解答
1,531 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carsten Bode,

As you mentioned, the L2 cache block is marked as optional in some i.MX6UL Part Numbers. The G0 version of the i.MX6UL is the less equipped of the i.MX6UL processors and indeed does not have L2 Cache so the information on the Fact Sheet is correct. If this is a requirement for your design I would recommend using the G1 version.

I hope this information helps!

在原帖中查看解决方案

3 回复数
1,532 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carsten Bode,

As you mentioned, the L2 cache block is marked as optional in some i.MX6UL Part Numbers. The G0 version of the i.MX6UL is the less equipped of the i.MX6UL processors and indeed does not have L2 Cache so the information on the Fact Sheet is correct. If this is a requirement for your design I would recommend using the G1 version.

I hope this information helps!

1,531 次查看
CarstenBode
Contributor II

Hello gusarambulo,

ok, thanks for the clarification, I understand that the L2 cache block is missing.

I assume the SCU is still present because it is separate from the L2C on the Corte A7.

Best regards

Carsten

1,531 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carsten Bide,

You are correct, the SCU is still present even if no L2 cache is available.

Regards,