Kitkat proxy issue in imx6 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kitkat proxy issue in imx6 board

1,694 Views
amit004
Contributor I

Hi, we are using imx6 board for our development and I am having some problem with the proxy setting. I see that if we open ethernet setting imx app and set the proxy it works.If we reboot the device it stops working. If we again launch the ethernet app and without doing anything just close, it will start working. If reboot again wont work. Did you guys see this issue or similar issue in kitkat.

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

1,518 Views
haoranwang
NXP Employee
NXP Employee

Hi Kumar,

     Freescale Android kitkat Ethernet APK will removed the proxy when the apk "onDestory". You can see this in the source code.

Thanks.

0 Kudos
Reply

1,518 Views
amit004
Contributor I

Hi

I am sorry I am not able to understand you. I found that when we reboot we don't broadcast proxy settings in connectivity service even though proxy is set. By broadcasting the proxy while loading proxy setting solved the problem.


Thanks

Amit

0 Kudos
Reply