Keymap calculation in IMX6 Sololite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keymap calculation in IMX6 Sololite

2,276 Views
himabindu
Contributor III

Hi Team,

            Currently I am  working on IMX6 Sololite Linux Kernel Version 3.10.17.Can you help me in calculating the Linux keymap present in DTS file for gpio-matrix keypad driver.

Thanks & Regards,

C.Himabindu.

Labels (1)
0 Kudos
Reply
2 Replies

2,079 Views
himabindu
Contributor III

Hi Team,

 

                 If we dont understand the logic implemented in Matrix Keymap present in dts file we can use the following Method to initialize the

keys in dts file . This integration requires two header files namely

#include "input.h"
#include "input-event-codes.h"

                             linux,keymap = <
                        KEY(0, 0, KEY_Q)
                        KEY(0, 1, KEY_I)
                        KEY(0, 2, KEY_G)
                        KEY(0, 3, KEY_C)
                        KEY(0, 4, KEY_TAB)
                        KEY(0, 5, KEY_4)
                        KEY(0, 6, KEY_8)
                        KEY(0, 7, KEY_ENTER)
                        KEY(1, 0, KEY_W)
                        KEY(1, 1, KEY_O)
                        KEY(1, 2, KEY_H)
                        KEY(1, 3, KEY_V)
                        KEY(1, 4, KEY_1)
                        KEY(1, 5, KEY_5)
                        KEY(1, 6, KEY_9)
                        KEY(1, 7, KEY_RESERVED)
                      >;


Thanks & Regards,

C.Himabindu.

0 Kudos
Reply

2,076 Views
igorpadykov
NXP Employee
NXP Employee

Hi Himabindu

explanation linux keypad can be found on

4x4 Matrix keypad Interfacing with i-MX6 - Toradex Community 

also may be useful attached Linux Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------