Kernel startup error encountered on iMX6S

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel startup error encountered on iMX6S

1,218 次查看
dinghui1111
Contributor I

We use MCIMX6S1AVM08AB on a board, and the u-boot(2015.04) and zImage(4.1.15) run ok on this board. Then we change the CPU to the model MCIMX6S6AVM08AD, but the same zImage can't work on it. 

The only difference of the two boards is the CPU model. All other hardware and software are the same. And the two CPUs are the same series. Because the MCIMX6S1AVM08AB is not recommended for new design, so we use the MCIMX6S6AVM08AD instead. Why this problem happen?

The attachment is the kernel early debug information.

标签 (1)
0 项奖励
回复
1 回复

1,139 次查看
igorpadykov
NXP Employee
NXP Employee

Hi hui

one can try ddr test and update image with new ddr calibration coefficients

(update in uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg)

i.MX6/7 DDR Stress Test Tool V2.92 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复