Kernel panic when using cpio.gz.u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel panic when using cpio.gz.u-boot

2,456 Views
raymondman
Contributor II

Our custom board is using iMX8MM with 1GB LPDDR4. Yocto is HardKnott version. We want to use example_kernel_emmc.uuu to program the custom board. The RAM size and the lpddr4 timing have been updated in both U-boot and kernel. However, the cpio.gz.u-boot produced by "bitbake fsl-image-mfgtool-initramfs" does not work. Below is the log. (We also use NXP pre-built file to test, but get the same kernel panic.) Please advise.

U-Boot SPL 2021.04-5.10.35-2.0.0+g3463140881 (Jan 26 2022 - 13:02:27 +0800)
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from USB SDP
g_dnl_register: g_dnl_driver.name = usb_dnl_sdp
g_dnl_bind: gadget: 0x7f9398 cdev: 0x42200490
usb_add_config: adding config #1 'usb_dnload'/42200540
g_dnl_do_config: configuration: 0x42200540 composite dev: 0x42200490
adding 'sdp'/42200680 to config 'usb_dnload'/42200540
cfg 1/42200540 speeds: high full
usb_add_config: interface 0 = sdp/42200680
g_dnl_bind: calling usb_gadget_connect for controller 'ci_udc'
usb_dnl_sdp: ready
SDP: initialize...
set_config: high speed config #1: usb_dnload
non-core control req21.0a v0000 i0000 l0
non-core control req81.06 v2200 i0000 l140
SDP: handle requests...
Downloading file of size 1148688 to 0x40400000... done
Jumping to header at 0x40400000
Header Tag is not an IMX image
Found header at 0x40428ba0
NOTICE: BL31: v2.2(release):rel_imx_5.4.70_2.3.2_rc1-0-g2a2678646
NOTICE: BL31: Built : 08:21:41, Jan 20 2022


U-Boot 2021.04-5.10.35-2.0.0+g3463140881 (Jan 26 2022 - 13:02:27 +0800)

alloc space exhausted
CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 52C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 1 GiB
tcpc_init: Can't find device id=0x52
setup_typec: tcpc port2 init failed, err=-19
tcpc_init: Can't find device id=0x50
setup_typec: tcpc port1 init failed, err=-19
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

In: serial
Out: serial
Err: serial
SEC0: RNG instantiated

BuildInfo:
- ATF 2a26786

MMC: no card present
Detect USB boot. Will enter fastboot mode!
Net: Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
No ethernet found.

Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for mfgtools
, using default environment

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0

## Checking Image at 43800000 ...
Legacy image found
Image Name: fsl-image-mfgtool-initramfs-imx8
Created: 2011-04-05 23:00:00 UTC
Image Type: AArch64 Linux RAMDisk Image (uncompressed)
Data Size: 14921573 Bytes = 14.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... Bad Data CRC
Run fastboot ...
g_dnl_register: g_dnl_driver.name = usb_dnl_fastboot
g_dnl_bind: gadget: 0x000000007ffc2b18 cdev: 0x000000007df1af90
usb_add_config: adding config #1 'usb_dnload'/000000007df1b040
g_dnl_do_config: configuration: 0x000000007df1b040 composite dev: 0x000000007df1af90
adding 'f_fastboot'/000000007df1b180 to config 'usb_dnload'/000000007df1b040
cfg 1/000000007df1b040 speeds: high full
usb_add_config: interface 0 = f_fastboot/000000007df1b180
g_dnl_bind: calling usb_gadget_connect for controller 'ci_udc'
usb_dnl_fastboot: ready
set_config: high speed config #1: usb_dnload
Detect USB boot. Will enter fastboot mode!
flash target is MMC:1
MMC: no card present
MMC card init failed!
MMC: no card present
** Block device MMC 1 not supported
Detect USB boot. Will enter fastboot mode!
flash target is MMC:2
Starting download of 1341296 bytes
..........
downloading of 1341296 bytes finished
writing to partition 'bootloader'
Initializing 'bootloader'
switch to partitions #1, OK
mmc2(part 1) is current device
Writing 'bootloader'

MMC write: dev # 2, block # 66, count 2620 ... 2620 blocks written: OK
Writing 'bootloader' DONE!
Detect USB boot. Will enter fastboot mode!
Detect USB boot. Will enter fastboot mode!
Detect USB boot. Will enter fastboot mode!
Detect USB boot. Will enter fastboot mode!
Detect USB boot. Will enter fastboot mode!
Detect USB boot. Will enter fastboot mode!
Starting download of 29491712 bytes
..........................................................................
..........................................................................
..........................................................................
...
downloading of 29491712 bytes finished
Detect USB boot. Will enter fastboot mode!
Starting download of 40863 bytes

downloading of 40863 bytes finished
Detect USB boot. Will enter fastboot mode!
Starting download of 14921637 bytes
..........................................................................
.......................................
downloading of 14921637 bytes finished
Detect USB boot. Will enter fastboot mode!
Moving Image from 0x40480000 to 0x40600000, end=422b0000
## Loading init Ramdisk from Legacy Image at 43800000 ...
Image Name: fsl-image-mfgtool-initramfs-imx8
Created: 2011-04-05 23:00:00 UTC
Image Type: AArch64 Linux RAMDisk Image (uncompressed)
Data Size: 14921573 Bytes = 14.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300cf9e

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.35+gef3f2cfc6010 (micom@micom-ESPRIMO-E420) (aarch64-poky-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.36.1.20210209) #31 SMP PREEMPT Thu Apr 14 17:01:22 HKT 2022
[ 0.000000] Machine model: FSL i.MX8MM EVK board
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma'
[ 0.000000] cma: Reserved 32 MiB at 0x000000007e000000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x000000007fffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x7ddd1700-0x7ddd3fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x000000007fffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x000000007fffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x000000007fffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 23 pages/cpu s56280 r8192 d29736 u94208
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258048
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc1,115200,115200 rdinit=/linuxrc clk_ignore_unused
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 951284K/1048576K available (17536K kernel code, 1472K rwdata, 6780K rodata, 2880K init, 545K bss, 64524K reserved, 32768K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] random: get_random_bytes called from start_kernel+0x330/0x4f4 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000004] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.000293] Console: colour dummy device 80x25
[ 0.000364] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.000377] pid_max: default: 32768 minimum: 301
[ 0.000442] LSM: Security Framework initializing
[ 0.000492] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.000504] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.001750] rcu: Hierarchical SRCU implementation.
[ 0.002586] EFI services will not be available.
[ 0.002756] smp: Bringing up secondary CPUs ...
[ 0.003106] Detected VIPT I-cache on CPU1
[ 0.003132] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.003178] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.003584] Detected VIPT I-cache on CPU2
[ 0.003602] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.003627] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.004054] Detected VIPT I-cache on CPU3
[ 0.004072] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.004094] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.004150] smp: Brought up 1 node, 4 CPUs
[ 0.004163] SMP: Total of 4 processors activated.
[ 0.004172] CPU features: detected: 32-bit EL0 Support
[ 0.004178] CPU features: detected: CRC32 instructions
[ 0.004186] CPU features: detected: 32-bit EL1 Support
[ 0.012510] CPU: All CPU(s) started at EL2
[ 0.012533] alternatives: patching kernel code
[ 0.013650] devtmpfs: initialized
[ 0.018811] KASLR disabled due to lack of seed
[ 0.018970] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.018985] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.020109] pinctrl core: initialized pinctrl subsystem
[ 0.020619] DMI not present or invalid.
[ 0.021011] NET: Registered protocol family 16
[ 0.027856] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[ 0.028754] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.029628] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.029721] audit: initializing netlink subsys (disabled)
[ 0.029954] audit: type=2000 audit(0.028:1): state=initialized audit_enabled=0 res=1
[ 0.030517] thermal_sys: Registered thermal governor 'step_wise'
[ 0.030521] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.030719] cpuidle: using governor menu
[ 0.030887] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.030968] ASID allocator initialised with 65536 entries
[ 0.031757] Serial: AMBA PL011 UART driver
[ 0.031813] imx mu driver is registered.
[ 0.031835] imx rpmsg driver is registered.
[ 0.054775] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/pdmgrp
[ 0.054803] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai1grp
[ 0.054819] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai1grp_dsd
[ 0.054837] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai2grp
[ 0.054851] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai3grp
[ 0.054867] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai5grp
[ 0.054912] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/usdhc2grpgpiogrp
[ 0.054940] imx8mm-pinctrl 30330000.pinctrl: no fsl,pins and pins property in node /soc@0/bus@30000000/pinctrl@30330000/lexi-imx8mm-gpio
[ 0.054965] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.071087] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.071101] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.071109] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.071117] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.072033] cryptd: max_cpu_qlen set to 1000
[ 0.074923] ACPI: Interpreter disabled.
[ 0.075463] iommu: Default domain type: Translated
[ 0.075606] vgaarb: loaded
[ 0.075908] SCSI subsystem initialized
[ 0.076217] usbcore: registered new interface driver usbfs
[ 0.076251] usbcore: registered new interface driver hub
[ 0.076277] usbcore: registered new device driver usb
[ 0.077251] mc: Linux media interface: v0.10
[ 0.077291] videodev: Linux video capture interface: v2.00
[ 0.077356] pps_core: LinuxPPS API ver. 1 registered
[ 0.077363] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 0.077377] PTP clock support registered
[ 0.077505] EDAC MC: Ver: 3.0.0
[ 0.078412] FPGA manager framework
[ 0.078486] Advanced Linux Sound Architecture Driver Initialized.
[ 0.079066] Bluetooth: Core ver 2.22
[ 0.079094] NET: Registered protocol family 31
[ 0.079100] Bluetooth: HCI device and connection manager initialized
[ 0.079112] Bluetooth: HCI socket layer initialized
[ 0.079121] Bluetooth: L2CAP socket layer initialized
[ 0.079136] Bluetooth: SCO socket layer initialized
[ 0.079752] clocksource: Switched to clocksource arch_sys_counter
[ 0.080034] VFS: Disk quotas dquot_6.6.0
[ 0.080081] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.080253] pnp: PnP ACPI: disabled
[ 0.085882] NET: Registered protocol family 2
[ 0.086255] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.086280] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.086366] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)
[ 0.086480] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.086559] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.086586] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.086697] NET: Registered protocol family 1
[ 0.086983] RPC: Registered named UNIX socket transport module.
[ 0.086989] RPC: Registered udp transport module.
[ 0.086995] RPC: Registered tcp transport module.
[ 0.087002] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.087702] PCI: CLS 0 bytes, default 64
[ 0.087899] Unpacking initramfs...
[ 0.795563] Freeing initrd memory: 14564K
[ 0.796278] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.796858] kvm [1]: IPA Size Limit: 40 bits
[ 0.798192] kvm [1]: GICv3: no GICV resource entry
[ 0.798198] kvm [1]: disabling GICv2 emulation
[ 0.798218] kvm [1]: GIC system register CPU interface enabled
[ 0.798287] kvm [1]: vgic interrupt IRQ9
[ 0.798399] kvm [1]: Hyp mode initialized successfully
[ 0.801376] Initialise system trusted keyrings
[ 0.801510] workingset: timestamp_bits=42 max_order=18 bucket_order=0
[ 0.806983] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.807567] NFS: Registering the id_resolver key type
[ 0.807594] Key type id_resolver registered
[ 0.807600] Key type id_legacy registered
[ 0.807675] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.807682] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.807702] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.808075] 9p: Installing v9fs 9p2000 file system support
[ 0.845249] Key type asymmetric registered
[ 0.845258] Asymmetric key parser 'x509' registered
[ 0.845293] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.845301] io scheduler mq-deadline registered
[ 0.845306] io scheduler kyber registered
[ 0.850226] EINJ: ACPI disabled.
[ 0.858724] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.858740] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.866343] mxs-dma 33000000.dma-controller: initialized
[ 0.868105] Bus freq driver module loaded
[ 0.873263] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.875356] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 39, base_baud = 1500000) is a IMX
[ 0.875992] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 40, base_baud = 5000000) is a IMX
[ 0.876518] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 41, base_baud = 1500000) is a IMX
[ 1.963903] printk: console [ttymxc1] enabled
[ 1.968768] Internal error: synchronous external abort: 96000210 [#1] PREEMPT SMP
[ 1.976251] Modules linked in:
[ 1.979314] CPU: 3 PID: 1 Comm: swapper/0 Not tainted 5.10.35+gef3f2cfc6010 #31
[ 1.986622] Hardware name: FSL i.MX8MM EVK board (DT)
[ 1.991675] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--)
[ 1.997688] pc : imx_uart_probe+0x2c0/0x7e4
[ 2.001873] lr : imx_uart_probe+0x2b0/0x7e4
[ 2.006055] sp : ffff800011cdbb50
[ 2.009369] x29: ffff800011cdbb50 x28: 0000000000000000
[ 2.014686] x27: ffff8000117e04e0 x26: ffff00000634b400
[ 2.020003] x25: 00000000fffffffa x24: 00000000fffffffa
[ 2.025321] x23: 000000000000002d x22: ffff000006291810
[ 2.030636] x21: ffff000006291800 x20: 0000000000000000
[ 2.035951] x19: ffff000006952080 x18: 0000000000000020
[ 2.041266] x17: 0000000000000000 x16: 0000000000000001
[ 2.046581] x15: ffff000006080478 x14: ffffffffffffffff
[ 2.051896] x13: 0000000000000038 x12: 0101010101010101
[ 2.057214] x11: 0000000000000020 x10: 0101010101010101
[ 2.062531] x9 : 0000000000000000 x8 : ffff00000634b500
[ 2.067846] x7 : 0000000000000000 x6 : 000000000000003f
[ 2.073161] x5 : 0000000000000080 x4 : 0000000000000000
[ 2.078476] x3 : 0000000000000000 x2 : 0000000000000000
[ 2.083791] x1 : ffff800012480080 x0 : 0000000000000000
[ 2.089106] Call trace:
[ 2.091555] imx_uart_probe+0x2c0/0x7e4
[ 2.095394] platform_drv_probe+0x54/0xb0
[ 2.099404] really_probe+0xe4/0x4c0
[ 2.102981] driver_probe_device+0x58/0xc0
[ 2.107079] device_driver_attach+0xc0/0xd0
[ 2.111263] __driver_attach+0x84/0x124
[ 2.115100] bus_for_each_dev+0x70/0xc0
[ 2.118938] driver_attach+0x24/0x30
[ 2.122514] bus_add_driver+0x104/0x1ec
[ 2.126350] driver_register+0x78/0x130
[ 2.130186] __platform_driver_register+0x4c/0x60
[ 2.134893] imx_uart_init+0x3c/0x64
[ 2.138470] do_one_initcall+0x54/0x1bc
[ 2.142309] kernel_init_freeable+0x1d4/0x23c
[ 2.146667] kernel_init+0x14/0x118
[ 2.150158] ret_from_fork+0x10/0x30
[ 2.153738] Code: 2a0003f4 35001d40 f9400a61 91020021 (b9400021)
[ 2.159842] ---[ end trace d132e31f7226938a ]---
[ 2.164506] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 2.172164] SMP: stopping secondary CPUs
[ 2.176092] Kernel Offset: disabled
[ 2.179581] CPU features: 0x0240002,2000200c
[ 2.183850] Memory Limit: none
[ 2.186908] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b ]---

0 Kudos
Reply
1 Reply

2,185 Views
oprata
Contributor II

Hi!

I have a custom board with 1G LPDDR4. I made some custom on dts. The release used was 5.15.32-2.0.0. The system works except of:

[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma'

If you fix your problem I really appreciate any tips.

Thanks in advance.

0 Kudos
Reply