Kernel panic when entering KGDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel panic when entering KGDB

2,704件の閲覧回数
972931182
Contributor I

Hi,

I'm trying to enable KGDB in linux-imx kernel for debugging. I did the following steps:

  1. git clone the source code from here: https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/configs?h=imx_5.4.3_2.0.0 
  2. checkout branch to imx_4.1.14_2.0.0_ga
  3. run make imx_v7_defconfig ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
  4. run make menuconfig ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- and enable these:
    --- KGDB: kernel debugger
        <*> KGDB: use kgdb over the serial console
        [ ] KGDB: internal test suite
        [*] KGDB_KDB: include kdb frontend for kgdb
        (0x1) KDB: Select kdb command functions to be enabled by default
        [ ] KGDB_KDB: keyboard as input device
        (0) KDB: continue after catastrophic errors
  5. run make zImage ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
  6. download zImage to my board
  7. restart board and enter in system
  8. run echo ttymxc1,9600 > /sys/module/kgdboc/parameters/kgdboc to register KGDBOC serial
  9. run echo g > /proc/sysrq-trigger to enter KGDB
  10. kernel panic shows 

The panic info is blew:

 

[   74.652531] sysrq: SysRq : DEBUG
[   74.655892] Unhandled fault: imprecise external abort (0x1c06) at 0x76ee328c
[   74.662958] pgd = 8866c000
[   74.665676] [76ee328c] *pgd=88644831, *pte=830f259f, *ppte=830f2e7e
[   74.672018] Internal error: : 1c06 [#1] PREEMPT SMP ARM
[   74.677294] KGDB: re-enter exception: ALL breakpoints killed
[   74.682969] ---[ end trace d61e9a1fd52b50df ]---
[   74.687606] Unhandled fault: imprecise external abort (0x1c06) at 0x76ee328c
[   74.694664] pgd = 8866c000
[   74.697382] [76ee328c] *pgd=88644831, *pte=830f259f, *ppte=830f2e7e
[   74.703711] Internal error: : 1c06 [#2] PREEMPT SMP ARM
[   74.708992] CPU: 0 PID: 152 Comm: sh Tainted: G      D         4.1.15-00158-g30278abfe097-dirty #1
[   74.717959] Hardware name: Freescale i.MX6 Ultralite (Device Tree)
[   74.724191] [<800161e0>] (unwind_backtrace) from [<80012748>] (show_stack+0x10/0x14)
[   74.731967] [<80012748>] (show_stack) from [<80809434>] (dump_stack+0x84/0xc4)
[   74.739220] [<80809434>] (dump_stack) from [<8009d8fc>] (kgdb_handle_exception+0x1fc/0x20c)
[   74.747600] [<8009d8fc>] (kgdb_handle_exception) from [<800157dc>] (kgdb_notify+0x24/0x3c)
[   74.755891] [<800157dc>] (kgdb_notify) from [<8004fe04>] (notifier_call_chain+0x44/0x84)
[   74.764010] [<8004fe04>] (notifier_call_chain) from [<80050088>] (atomic_notifier_call_chain+0x34/0x48)
[   74.773429] [<80050088>] (atomic_notifier_call_chain) from [<80050608>] (notify_die+0x38/0x40)
[   74.782066] [<80050608>] (notify_die) from [<80012848>] (die+0xfc/0x3f0)
[   74.788789] [<80012848>] (die) from [<80009304>] (do_DataAbort+0xb4/0xb8)
[   74.795600] [<80009304>] (do_DataAbort) from [<800131d8>] (__dabt_svc+0x38/0x60)
[   74.803009] Exception stack(0x88799be0 to 0x88799c28)
[   74.808082] 9be0: 8829c410 0000000a 00005008 a0950000 80c57f19 80c57f18 80c57f18 0000002b
[   74.816279] 9c00: 80c589d8 80c58ae8 80c53aac 00000000 881bd000 88799c28 8009f838 803618d0
[   74.824467] 9c20: 000d0093 ffffffff
[   74.827987] [<800131d8>] (__dabt_svc) from [<803618d0>] (imx_poll_put_char+0x20/0x2c)
[   74.835844] [<803618d0>] (imx_poll_put_char) from [<8009f838>] (vkdb_printf+0x1d4/0xa30)
[   74.843961] [<8009f838>] (vkdb_printf) from [<800a00b8>] (kdb_printf+0x24/0x34)
[   74.851296] [<800a00b8>] (kdb_printf) from [<800a41b0>] (kdb_main_loop+0x100/0x7d0)
[   74.858974] [<800a41b0>] (kdb_main_loop) from [<800a7080>] (kdb_stub+0x2ac/0x508)
[   74.866480] [<800a7080>] (kdb_stub) from [<8009d2e0>] (kgdb_cpu_enter+0x414/0x710)
[   74.874073] [<8009d2e0>] (kgdb_cpu_enter) from [<8009d7f8>] (kgdb_handle_exception+0xf8/0x20c)
[   74.882707] [<8009d7f8>] (kgdb_handle_exception) from [<80015790>] (kgdb_compiled_brk_fn+0x28/0x30)
[   74.891774] [<80015790>] (kgdb_compiled_brk_fn) from [<800090f8>] (do_undefinstr+0xe4/0x190)
[   74.900231] [<800090f8>] (do_undefinstr) from [<800132ec>] (__und_svc_finish+0x0/0x34)
[   74.908159] Exception stack(0x88799e70 to 0x88799eb8)
[   74.913226] 9e60:                                     00000067 80a485c4 00000000 00000000
[   74.921422] 9e80: 80c53aa0 80c53aa4 80b9a504 00000067 00000000 88798000 00000000 013f7008
[   74.929614] 9ea0: 00000000 88799eb8 8034fa1c 8009c884 600d0013 ffffffff
[   74.936251] [<800132ec>] (__und_svc_finish) from [<8009c884>] (kgdb_breakpoint+0x44/0x78)
[   74.944454] [<8009c884>] (kgdb_breakpoint) from [<8034fa1c>] (__handle_sysrq+0xac/0x178)
[   74.952570] [<8034fa1c>] (__handle_sysrq) from [<8034ff14>] (write_sysrq_trigger+0x38/0x48)
[   74.960951] [<8034ff14>] (write_sysrq_trigger) from [<80146c64>] (proc_reg_write+0x5c/0x84)
[   74.969330] [<80146c64>] (proc_reg_write) from [<800f4e10>] (__vfs_write+0x20/0xdc)
[   74.977011] [<800f4e10>] (__vfs_write) from [<800f55ec>] (vfs_write+0x90/0x164)
[   74.984345] [<800f55ec>] (vfs_write) from [<800f5e10>] (SyS_write+0x44/0x9c)
[   74.991419] [<800f5e10>] (SyS_write) from [<8000f480>] (ret_fast_syscall+0x0/0x3c)
[   74.999003] Kernel panic - not syncing: Recursive entry to debugger

 

----------------------------------------------------------------------------------------------------------------

Probably solution

 

It seems that there may be some errors in the functionimx_poll_putchar.After several nights of debugging, I have found that this panic is caused because the TXEN bit in UCR2 register for uart2(ttymxc1) is not enable. 

And I think which should be enable in imx_poll_init:

 

static int imx_poll_init(struct uart_port *port)
{
	struct imx_port *sport = (struct imx_port *)port;
	unsigned long flags;
	unsigned long temp;
	int retval;

	retval = clk_prepare_enable(sport->clk_ipg);
	if (retval)
		return retval;
	retval = clk_prepare_enable(sport->clk_per);
	if (retval)
		clk_disable_unprepare(sport->clk_ipg);

	imx_setup_ufcr(sport, 0);

	spin_lock_irqsave(&sport->port.lock, flags);

	temp = readl(sport->port.membase + UCR1);
	if (is_imx1_uart(sport))
		temp |= IMX1_UCR1_UARTCLKEN;
	temp |= UCR1_UARTEN | UCR1_RRDYEN;
	temp &= ~(UCR1_TXMPTYEN | UCR1_RTSDEN);
	writel(temp, sport->port.membase + UCR1);

	temp = readl(sport->port.membase + UCR2);
	temp |= UCR2_RXEN;
	writel(temp, sport->port.membase + UCR2);

	spin_unlock_irqrestore(&sport->port.lock, flags);

	return 0;
}

 

At the fourth to last line, maybe should aslo enable UCR2_TXEN . like this:

 

temp |= (UCR2_RXEN | UCR2_TXEN);

 

After modify that line, my problem has been solved . I'm not sure if this is a bug.

I hope someone could check about this. And if this is a bug, I'd like to submit a patch or pull request to this.

Thanks.

0 件の賞賛
返信
2 返答(返信)

2,700件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 972931182

 

reason may be versions incompatibility of software components, so one can try

to rebuild all image from scratch using revisions described in Release Notes document for

each BSP on linux documentation link:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Recommended to try latest  Linux 5.4.47_2.2.0​​  i.MX Linux Release Notes

 

Best regards
igor

0 件の賞賛
返信

2,694件の閲覧回数
972931182
Contributor I

Thanks for your reply, I will try to use the latest Linux 5.4.47_2.2.0 and post the result at here later.

0 件の賞賛
返信