Kernel panic - not syncing: No init found.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel panic - not syncing: No init found.

7,108 Views
vishvapathi
Contributor V

Hi,

i am getting the below error, for testing purpose I download ready to use image from freescale web site and wrote into sd card memory ext2 partition which I created. I downloaded the Ubuntu Oneiric from freescale website.

Waiting for root device /dev/mmcblk1p1...

mmc2: new high speed SDHC card at address b368

mmcblk1: mmc2:b368 SDC   7.41 GiB

mmcblk1: p1

EXT3-fs: barriers not enabled

kjournald starting.  Commit interval 5 seconds

EXT3-fs (mmcblk1p1): using internal journal

EXT3-fs (mmcblk1p1): recovery complete

EXT3-fs (mmcblk1p1): mounted filesystem with writeback data mode

VFS: Mounted root (ext3 filesystem) on device 179:25.

Freeing init memory: 204K

Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.t.

[<80047834>] (unwind_backtrace+0x0/0xf8) from [<80508af4>] (panic+0x74/0x18c)

[<80508af4>] (panic+0x74/0x18c) from [<80508808>] (init_post+0xa0/0xc4)

[<80508808>] (init_post+0xa0/0xc4) from [<800089b4>] (kernel_init+0x10c/0x13c)

[<800089b4>] (kernel_init+0x10c/0x13c) from [<80041aa4>] (kernel_thread_exit+0x0/0x8)

CPU2: stopping

[<80047834>] (unwind_backtrace+0x0/0xf8) from [<8003b324>] (do_IPI+0x150/0x17c)

[<8003b324>] (do_IPI+0x150/0x17c) from [<80040a0c>] (__irq_svc+0x4c/0xe8)

Exception stack(0xbffb5ef0 to 0xbffb5f38)

5ee0:                                     bffb5f38 0000000a 00000000 00000002

5f00: 00000282 bffb4000 bffb4000 00000000 80af77e0 00000002 80a90040 00000000

5f20: 80047134 bffb5f38 8007a570 80079fd4 20000113 ffffffff

[<80040a0c>] (__irq_svc+0x4c/0xe8) from [<80079fd4>] (__do_softirq+0x4c/0x140)

[<80079fd4>] (__do_softirq+0x4c/0x140) from [<8007a570>] (irq_exit+0x94/0x9c)

[<8007a570>] (irq_exit+0x94/0x9c) from [<8003b2e0>] (do_IPI+0x10c/0x17c)

[<8003b2e0>] (do_IPI+0x10c/0x17c) from [<80040a0c>] (__irq_svc+0x4c/0xe8)

Exception stack(0xbffb5f90 to 0xbffb5fd8)                                               

5f80:                                     80af9140 80000093 00000001 00000000           

5fa0: bffb4000 80af1ce4 80510fa4 80aa6e7c 1000406a 412fc09a 00000000 00000000           

5fc0: 00000000 bffb5fd8 8004f648 80041b04 40000013 ffffffff                             

[<80040a0c>] (__irq_svc+0x4c/0xe8) from [<80041b04>] (default_idle+0x24/0x28)           

[<80041b04>] (default_idle+0x24/0x28) from [<80041d08>] (cpu_idle+0xc8/0x108)           

[<80041d08>] (cpu_idle+0xc8/0x108) from [<10505934>] (0x10505934)                       

CPU3: stopping                                                                          

[<80047834>] (unwind_backtrace+0x0/0xf8) from [<8003b324>] (do_IPI+0x150/0x17c)         

[<8003b324>] (do_IPI+0x150/0x17c) from [<80040a0c>] (__irq_svc+0x4c/0xe8)               

Exception stack(0xbff01f90 to 0xbff01fd8)                                               

1f80:                                     80af9140 80000093 00000001 00000000           

1fa0: bff00000 80af1ce4 80510fa4 80aa6e7c 1000406a 412fc09a 00000000 00000000           

1fc0: 00000000 bff01fd8 8004f648 80041b04 40000013 ffffffff                             

[<80040a0c>] (__irq_svc+0x4c/0xe8) from [<80041b04>] (default_idle+0x24/0x28)           

[<80041b04>] (default_idle+0x24/0x28) from [<80041d08>] (cpu_idle+0xc8/0x108)           

[<80041d08>] (cpu_idle+0xc8/0x108) from [<10505934>] (0x10505934)                       

CPU1: stopping                                                                          

[<80047834>] (unwind_backtrace+0x0/0xf8) from [<8003b324>] (do_IPI+0x150/0x17c)         

[<8003b324>] (do_IPI+0x150/0x17c) from [<80040a0c>] (__irq_svc+0x4c/0xe8)               

Exception stack(0xbffadf90 to 0xbffadfd8)                                               

df80:                                     80af9140 60000093 00000001 00000000           

dfa0: bffac000 80af1ce4 80510fa4 80aa6e7c 1000406a 412fc09a 00000000 00000000

dfc0: 00000000 bffadfd8 8004f648 80041b04 40000013 ffffffff

[<80040a0c>] (__irq_svc+0x4c/0xe8) from [<80041b04>] (default_idle+0x24/0x28)

[<80041b04>] (default_idle+0x24/0x28) from [<80041d08>] (cpu_idle+0xc8/0x108)

[<80041d08>] (cpu_idle+0xc8/0x108) from [<10505934>] (0x10505934)

I checked the rootfs. It has /sbin/init, /etc/init files. I also tried pointing the init folder by setting environment, stil no difference.

How do i proceed. Any help would be appreciated.


Labels (2)
0 Kudos
Reply
7 Replies

3,374 Views
LeonardoSandova
Specialist I

Reformat your partition as EXT3 and place the rootfs again.

0 Kudos
Reply

3,374 Views
vishvapathi
Contributor V

I tried it already.. still the problem exists..... any other alternate for this!!! 

0 Kudos
Reply

3,374 Views
LeonardoSandova
Specialist I

Make sure the kernel supports either ext2, ext3 or ext4. (on the kernel menu, go to file sytems submenu). I would also try with another SD card with at least 4GB.

0 Kudos
Reply

3,374 Views
vishvapathi
Contributor V

Hi Leo,

After adding "rootfstype=ext3" to env i am able to login. Though i am getting below message before login.

"No space left on device" but its a 8gb SD card.

Starting the hotplug events dispatcher udevd                              

udevd (1437): /proc/1437/oom_adj is deprecated, please use /proc/1437/oom_score.

Synthesizing initial hotplug events                                       
Setting the hostname to freescale                                         
Mounting filesystems                                                      
cp: writing `/mnt/rwfs/var/lib/rpm/Packages': No space left on device     
cp: writing `/mnt/rwfs/var/lib/rpm/Filemd5s': No space left on device     
cp: writing `/mnt/rwfs/var/lib/rpm/Provideversion': No space left on device
cp: writing `/mnt/rwfs/var/lib/rpm/Name': No space left on device         
cp: writing `/mnt/rwfs/var/lib/rpm/Requirename': No space left on device  
cp: writing `/mnt/rwfs/var/lib/rpm/Conflictname': No space left on device 
cp: writing `/mnt/rwfs/var/lib/rpm/Sigmd5': No space left on device       
cp: writing `/mnt/rwfs/var/lib/rpm/Group': No space left on device        
cp: writing `/mnt/rwfs/var/lib/rpm/Dirnames': No space left on device     
cp: writing `/mnt/rwfs/var/lib/rpm/Basenames': No space left on device    
cp: writing `/mnt/rwfs/var/lib/rpm/Sha1header': No space left on device   

cp: writing `/mnt/rwfs/var/state/dhcp/dhcpd.leases': No space left on device   

cp: writing `/mnt/rwfs/var/state/dhcp/dhclient.leases': No space left on device

mount: mounting usbfs on /proc/bus/usb failed: No such file or directory  
Starting the port mapper:                                                 
Starting the dropbear ssh server:                                         

D-Bus per-session daemon address is: unix:abstract=/tmp/dbus-8evMBMKx7a,guid=269

gtk: creating gdk-pixbuf.loaders                                          
pango: creating module list                                               
starting pid 3278, tty '': '/etc/rc.d/rc_gpu.S'                           
starting pid 3286, tty '': '/etc/rc.d/rc_mxc.S'                           
                                                                          
_XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6          
_XSERVTransOpen: transport open failed for inet6/freescale:0              
_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6  

arm-none-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08)

root filesystem built on Tue, 02 Jul 2013 15:21:28 +0530                  
Freescale Semiconductor, Inc.                                             
                                                                          

freescale login: (EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/bae

(EE) XKB: No components provided for device Virtual core keyboard         
unrecognised device identifier!                                           
(EE) config/hal: NewInputDeviceRequest failed (2)                         
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <Alt>n=next                               
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <Alt>p=prev                               
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <Alt>c=close                              
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <Alt>d=desktop                            
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <Alt>m=!matchbox-remote -mbmenu           
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <ctrl><alt>x=!xterm                       
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <ctrl><alt>r=!rxvt                        
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <ctrl><alt>e=!!gpe-calender               
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <alt>Tab=next                             
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <alt><shift>Tab=prev                      
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <alt>space=taskmenu                       
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <alt>escape=!matchbox-remote -mbmenu      
                                                                          
matchbox: keyboard does not appear to have a <alt> key.                   
matchbox: ignoring key shortcut <alt>f4=close                             
                                                                          
matchbox: Cant find a keycode for keysym 65480                            
matchbox: ignoring key shortcut f11=fullscreen                            
                                                                          

matchbox-desktop: loading /usr/lib/matchbox/desktop/tasks.so with args ( None )

matchbox-desktop: loading /usr/lib/matchbox/desktop/dotdesktop.so with args ( N)

user_overides is (nil)                                                    
mb-desktop-dotdesktop: failed to open /usr/local/share/applications       
mb-desktop-dotdesktop: failed to open //.applications                     
mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name  
mb-applet-menu-launcher: failed to open /usr/local/share/applications     
mb-applet-menu-launcher: failed to open //.applications                   
mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name  
mb-applet-menu-launcher: failed to open /usr/local/share/applications     
mb-applet-menu-launcher: failed to open //.applications    


0 Kudos
Reply

3,374 Views
LeonardoSandova
Specialist I

For some reason, the /mnt/rwfs is not mounted. Try manually this

mount -t tmpfs rwfs /mnt/rwfs/


Also, there must be something not setting right on this file

/etc/rc.d/init.d/filesystems


0 Kudos
Reply

3,374 Views
vishvapathi
Contributor V

cat /etc/rc.d/init.d/filesystems

#!/bin/sh 

 

if [ "$1" = "stop" ]

then 

  echo Unmounting filesystems 

  umount -a -r 

  mount -o remount -r %root% / 

  [ -x /sbin/swapoff ] && swapoff -a

fi 

 

if [ "$1" = "start" ]

then 

  echo Mounting filesystems 

  if [ "$TMPFS" = "tmpfs" ]

  then 

  mount -n -t $TMPFS shm /dev/shm 

  fi 

  if [ -n "$TMPFS" ] 

  then 

  mount -n -t $TMPFS rwfs /mnt/rwfs -o size=$TMPFS_SIZE

  fi 

  if [ "$READONLY_FS" != "y" ]

  then 

  mount -n -o remount -w %root% / 

  NFSBOOT="`cat /proc/cmdline | grep -q /dev/nfs ; echo $?`"

  if [ "$NFSBOOT" == "0" -a -n "$RAMDIRS" ] 

  then 

  echo "Booted NFS, not relocating: $RAMDIRS"

  RAMDIRS="" 

  fi 

  else 

  # initramfs, ramdisks, others? come up read/write by default

  mount -n -o remount -r %root% / 

  RAMDIRS="$RAMDIRS /tmp /etc /var"

  fi 

  if [ -n "$RAMDIRS" ] 

  then 

  for i in $RAMDIRS 

  do 

  if [ ! -e /mnt/rwfs/$i ] 

  then 

  cp -a $i /mnt/rwfs/ 

  mount -n -o bind /mnt/rwfs/$i $i

  fi 

  done 

  fi 

  if [ -e /etc/mtab ] 

  then 

  rm -f /etc/mtab 

  fi 

  ln -s /proc/mounts /etc/mtab 

  if [ ! -d /dev/pts ] 

  then 

  mkdir /dev/pts 

  fi 

  mount -a 

fi 


i tried to mount manually but still i get no space during booting...


0 Kudos
Reply

3,374 Views
ronglinchen
Contributor I

Hi Kaman

I have the same problem like "mb-applet-menu-launcher: failed to open //.applications   ",

Have you solved it?

Please tell me if you got it ,THX very much!!

0 Kudos
Reply