Kernel panic - not syncing: Attempted to kill init!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel panic - not syncing: Attempted to kill init!

7,543件の閲覧回数
lifusong
Contributor IV

Dear sir.

our BSP is 5.0, kernel is 3.10.53  ,uboot 2014.04  and soc is imx6qsabresd 800MHz   pmic is DA9063.

if Add PMIC driver ONEKEY Support. when power down,we get below info,and the machine will restart.

SysRq : Emergency Remount R/O

EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)

EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)

Emergency Remount complete

imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!

Power down.

Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000000

and if remove ONEKEY support ,can't see this issue,but can't shutdown the power only shutdown android os.

how to fix this issue?

thanks all.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

6,393件の閲覧回数
jerinsebastian
Contributor I

I am also having the same issue. Did you resolve the issue li fusong??

0 件の賞賛
返信

6,393件の閲覧回数
lifusong
Contributor IV

No, we remove ONEKey Function and add gpio to controller the mainboard power

0 件の賞賛
返信

6,388件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi li

I would suggest to check if hardware can trigger PMIC reset,

as described in Table 19. Known Issues and Workarounds

attached document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信