Kernel panic - not syncing: Attempted to kill init!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel panic - not syncing: Attempted to kill init!

7,837 Views
lifusong
Contributor IV

Dear sir.

our BSP is 5.0, kernel is 3.10.53  ,uboot 2014.04  and soc is imx6qsabresd 800MHz   pmic is DA9063.

if Add PMIC driver ONEKEY Support. when power down,we get below info,and the machine will restart.

SysRq : Emergency Remount R/O

EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)

EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)

Emergency Remount complete

imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!

Power down.

Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000000

and if remove ONEKEY support ,can't see this issue,but can't shutdown the power only shutdown android os.

how to fix this issue?

thanks all.

Labels (3)
0 Kudos
Reply
3 Replies

6,687 Views
jerinsebastian
Contributor I

I am also having the same issue. Did you resolve the issue li fusong??

0 Kudos
Reply

6,687 Views
lifusong
Contributor IV

No, we remove ONEKey Function and add gpio to controller the mainboard power

0 Kudos
Reply

6,682 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

I would suggest to check if hardware can trigger PMIC reset,

as described in Table 19. Known Issues and Workarounds

attached document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply