Kernel Splash screen reg

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Splash screen reg

1,400件の閲覧回数
sachusanal
Contributor III

hello

I set a kernel splash screen in kernel image but it is loading so much late .I need to set splash screen in kernel which is loading at the time of kernel booting

please help me

ラベル(1)
0 件の賞賛
返信
1 返信

1,163件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Have you tried with a smaller image? Have you verified the initialization order? You could refer to the following threads from the Community:

Re: delay between the boot loader and kernel splash screens

boot time optimisation reg(kernel side)

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信