Keep same header structure in SRK Table and Record

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Keep same header structure in SRK Table and Record

3,950 次查看
csoapy
Contributor III

I'm writing code to parse container file. And found that there are 3 similar struct headers used to indicate data block's TAG, SIZE and VERSION:

A: { VERSION, LENGTH_L, LENGHT_H, TAG}

        Used in Container, SignatureBlock, Signature, Certificate, Block(DEK)'s header.

B: {TAG,  LENGTH_L/H, LENGHT_H/L, VERSION}

        Used in SRK Table's header.

C: {Tag, LENGTH_L/H, LENGHT_H/L}

        Used in SRK Record's header

P.S. I use `L/H` because there are labled as `Variable` in a fixed length of 2 bytes in i.MX8 RM Rev.0

This two make me confused:

  1. Why not use same structures?
  2. Why not place TAG to the first byte of a structure?
0 项奖励
回复
8 回复数

3,877 次查看
csoapy
Contributor III

Another weird order in Signature Block:

Offset:    {Certi,           SRK Table,  Sign, Blob}

Content: {SRK Table, Sign,            Certi, Blob}

csoapy_0-1600347575965.png

 

 

0 项奖励
回复

3,872 次查看
igorpadykov
NXP Employee
NXP Employee

processor ROM structures and definitions are hardcoded at chip design level,

they can not be changed later.

 

Best regards
igor

0 项奖励
回复

3,866 次查看
csoapy
Contributor III

processor ROM structures and definitions are hardcoded at chip design level,

they can not be changed later.

Since it's hardcoded, then hardcode them again.

I don't think they can not be changed later.

There're i.MX8 B0 and C0 release. So why can't fix them in D0?

It's about how much works need to be done.

It's not about CAN or CAN NOT.

BAD is BAD. and need to be fixed.

 

0 项奖励
回复

3,942 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

3,934 次查看
csoapy
Contributor III

@igorpadykov  Can you delete your reply? It's not an answer to the question.

0 项奖励
回复

3,921 次查看
igorpadykov
NXP Employee
NXP Employee

 answer to the questions:

  1. Why not use same structures?
  2. Why not place TAG to the first byte of a structure?
  3.  

A: it is defined in i.MX8 ROM.

 

Best regards
igor

0 项奖励
回复

3,898 次查看
csoapy
Contributor III

@igorpadykov  I mean, it's a bad definition, a bad design in another word.

0 项奖励
回复

3,890 次查看
igorpadykov
NXP Employee
NXP Employee

>I mean, it's a bad definition, a bad design in another word.

 

sorry processor ROM structures and definitions are hardcoded at chip design level,

they can not be changed later.

 

Best regards
igor

0 项奖励
回复