Keep boot logo from u-boot during kernel boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Keep boot logo from u-boot during kernel boot

1,653件の閲覧回数
david_schmidt
Contributor II

Hello,

during u-boot, I initialize the framebuffer of my i.MX6 board and display a logo.

The problem is as soon as kernel starts, screen turns black until framebuffer is initialized.

Is it possible to keep the framebuffer unchanged during kernel boot so I can keep the logo displayed?

Setting the boot logo during kernel boot is not possible because the boot logo needs to be dynamic and not statically compiled into kernel.

ラベル(2)
0 件の賞賛
返信
1 返信

1,647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi david_schmidt

 

one can try logo patches from

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-uboot-logo-keep-from-ub...

 

Best regards
igor

0 件の賞賛
返信