Keep boot logo from u-boot during kernel boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Keep boot logo from u-boot during kernel boot

1,188 次查看
david_schmidt
Contributor II

Hello,

during u-boot, I initialize the framebuffer of my i.MX6 board and display a logo.

The problem is as soon as kernel starts, screen turns black until framebuffer is initialized.

Is it possible to keep the framebuffer unchanged during kernel boot so I can keep the logo displayed?

Setting the boot logo during kernel boot is not possible because the boot logo needs to be dynamic and not statically compiled into kernel.

标签 (2)
0 项奖励
回复
1 回复

1,182 次查看
igorpadykov
NXP Employee
NXP Employee

Hi david_schmidt

 

one can try logo patches from

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-uboot-logo-keep-from-ub...

 

Best regards
igor

0 项奖励
回复