KSZ9031 interface with IMX6 Dual Processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSZ9031 interface with IMX6 Dual Processor

ソリューションへジャンプ
1,904件の閲覧回数
tejummb
Contributor II

Hi everyone,

We are using a custom board which has KSZ9031 phy interfaced with iMX6 dual processor.

The 125 MHz from PHY is not connected to ENET_REF_CLK (V22) of processor.

So, we are not able to succeed in the ethernet functionality test using platform SDK as well as u-boot.

Can anyone confirm whether it is possible to use the board the same way, or a board re-spin is required?

Regards,

Teju M M B

ラベル(5)
0 件の賞賛
返信
1 解決策
1,670件の閲覧回数
art
NXP Employee
NXP Employee

There is no way to run the RGMII interface without 125MHz reference clock from PHY, connected to the processor's ENET_REF_CLK input. This connection is mandatory. The hardware fix is required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,671件の閲覧回数
art
NXP Employee
NXP Employee

There is no way to run the RGMII interface without 125MHz reference clock from PHY, connected to the processor's ENET_REF_CLK input. This connection is mandatory. The hardware fix is required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信