KSZ9031 interface with IMX6 Dual Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSZ9031 interface with IMX6 Dual Processor

Jump to solution
1,900 Views
tejummb
Contributor II

Hi everyone,

We are using a custom board which has KSZ9031 phy interfaced with iMX6 dual processor.

The 125 MHz from PHY is not connected to ENET_REF_CLK (V22) of processor.

So, we are not able to succeed in the ethernet functionality test using platform SDK as well as u-boot.

Can anyone confirm whether it is possible to use the board the same way, or a board re-spin is required?

Regards,

Teju M M B

Labels (5)
0 Kudos
Reply
1 Solution
1,666 Views
art
NXP Employee
NXP Employee

There is no way to run the RGMII interface without 125MHz reference clock from PHY, connected to the processor's ENET_REF_CLK input. This connection is mandatory. The hardware fix is required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,667 Views
art
NXP Employee
NXP Employee

There is no way to run the RGMII interface without 125MHz reference clock from PHY, connected to the processor's ENET_REF_CLK input. This connection is mandatory. The hardware fix is required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply