Jump to Application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,680件の閲覧回数
saranbabu
Contributor II

Hello Team,

Here I've attached two files of memory configuration, both bootloader and application.  With this configuration it is not jump into the application.  It is continuously rebooting, please check and let me know the solution for this issue.

Application_memory_config.PNG

 

Bootloader_memory_config.PNG

 

Regards,

Saranbabu KM

 

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,659件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Please use the release configuration for building the bootloader.
The configuration is correct although I suggest you double-check it through the linker files.
It is also important to check that the bootable image is correct, you might refer to this AN: AN12238: i.MX RT Flashloader Use Case – Application Note (nxp.com)

Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,660件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Please use the release configuration for building the bootloader.
The configuration is correct although I suggest you double-check it through the linker files.
It is also important to check that the bootable image is correct, you might refer to this AN: AN12238: i.MX RT Flashloader Use Case – Application Note (nxp.com)

Best regards,
Omar

0 件の賞賛
返信