Jump to Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jump to Application

Jump to solution
1,660 Views
saranbabu
Contributor II

Hello Team,

Here I've attached two files of memory configuration, both bootloader and application.  With this configuration it is not jump into the application.  It is continuously rebooting, please check and let me know the solution for this issue.

Application_memory_config.PNG

 

Bootloader_memory_config.PNG

 

Regards,

Saranbabu KM

 

 

 

Tags (1)
0 Kudos
Reply
1 Solution
1,639 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Please use the release configuration for building the bootloader.
The configuration is correct although I suggest you double-check it through the linker files.
It is also important to check that the bootable image is correct, you might refer to this AN: AN12238: i.MX RT Flashloader Use Case – Application Note (nxp.com)

Best regards,
Omar

View solution in original post

0 Kudos
Reply
1 Reply
1,640 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Please use the release configuration for building the bootloader.
The configuration is correct although I suggest you double-check it through the linker files.
It is also important to check that the bootable image is correct, you might refer to this AN: AN12238: i.MX RT Flashloader Use Case – Application Note (nxp.com)

Best regards,
Omar

0 Kudos
Reply