JTAG programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG programmer

13,067件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

I wonder what JTAG programmer that is recommended to the i.MX6?

Also what tool would you recommend to do the debugging?

Thanks,

Niklas

ラベル(3)
0 件の賞賛
返信
6 返答(返信)

6,947件の閲覧回数
rtsiexpert
Contributor I

I am using the Macraigor USB Wiggler JTAG.  Pretty basic, but it seems to be enough to bring up a board with some software.    The do support GCC & Eclipse for development.

0 件の賞賛
返信

6,947件の閲覧回数
niklasmolin
Senior Contributor I

Hi Allan.

This looks more like what I'm after.

Are you using it for I.mx6?

What software are you using then to download code?

Thanks,

Niklas

0 件の賞賛
返信

6,947件の閲覧回数
rtsiexpert
Contributor I

Niklas

   Yes I am working with the i.mx53 and I.mx6 Quad.    The i.mx6 is the Win Systems board.   I am using the u-boot to download OS-9 RTOS.   I am porting it to run on these chips.   I have it running now on the i.mx53, and the i.mx6 should be running in the next few days.  Once I get the OS and basic boot code working, I then plan to figure out to use the booter code to replace the u-boot.

Allan

0 件の賞賛
返信

6,947件の閲覧回数
sinanakman
Senior Contributor III

Hi Niklas, in addition to the list provided above, there is also BDI3000 from Abatron AG that we regularly use with iMX6.

Hope this helps

Sinan Akman

0 件の賞賛
返信

6,947件の閲覧回数
niklasmolin
Senior Contributor I

Thanks,

I'll check this.

Right now I'm trying to find something that is not too fancy since we'll mostly use it incase we can't get the Processor up and running, when we get the board.

Thanks,

Niklas

0 件の賞賛
返信

6,947件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

   Generally the following summary link contains information about recommended tools.
Please look at sections "Hardware Development Tools".      

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

Please consult with JTAG tool / probe provider about i.MX6 initialization scripts.

Also  please pay attention :

The JTAG_MOD pin of the JTAG connector controls the selection of JTAG to the core logic or

boundary scan operation. For software debugging The JTAG_MOD should be pulled

down.

2.

ARM RealView and DS-5 support i.MX6.

http://www.arm.com/products/tools/software-tools/ds-5/index.php

http://www.arm.com/products/tools/software-tools/rvds/index.php

The  next JTAG probes may be applied : RealView  ICE and  DSTREAM.

http://www.arm.com/products/tools/debug-adapters/rvi-rvt2.php


Also please find an overview of 3rd party development tools for ARM here:

http://www.freescale.com/files/wireless_comm/doc/brochure/BRTOOLENABLECO.pdf

The next app note may be useful in debugging :

"AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors."

http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf