JTAG has no access to imx6dl sabresd ddr.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG has no access to imx6dl sabresd ddr.

1,139件の閲覧回数
wenmingfeng
Contributor III

Hi chip expertise,

When I setup our customer board same schematic with imx6dl sabresd, I got below error.

This means, I have no access read/write the ddrs. Someone can give some debugging method.

load_image u-boot-0x27800000_imx6dl_20160410.bin 0x27800000
JTAG-DP STICKY ERROR
MEM_AP_CSW 0x428000e2, MEM_AP_TAR 0x21b001c
Failed to write memory at 0x021b001c
embedded:startup.tcl:21: Error:
in procedure 'imx6.cpu.0'
in procedure 'ocd_bouncer'
at file "embedded:startup.tcl", line 21

Thanks!

Wenming

0 件の賞賛
返信
2 返答(返信)

933件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wenming

for ocd usage one can check

Using JTAG for imx6 board bringup 

Problems in i.mx6 board with openocd 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

933件の閲覧回数
wenmingfeng
Contributor III

Thanks igor!

0 件の賞賛
返信