JTAG has no access to imx6dl sabresd ddr.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG has no access to imx6dl sabresd ddr.

1,116 Views
wenmingfeng
Contributor III

Hi chip expertise,

When I setup our customer board same schematic with imx6dl sabresd, I got below error.

This means, I have no access read/write the ddrs. Someone can give some debugging method.

load_image u-boot-0x27800000_imx6dl_20160410.bin 0x27800000
JTAG-DP STICKY ERROR
MEM_AP_CSW 0x428000e2, MEM_AP_TAR 0x21b001c
Failed to write memory at 0x021b001c
embedded:startup.tcl:21: Error:
in procedure 'imx6.cpu.0'
in procedure 'ocd_bouncer'
at file "embedded:startup.tcl", line 21

Thanks!

Wenming

0 Kudos
Reply
2 Replies

910 Views
igorpadykov
NXP Employee
NXP Employee

Hi wenming

for ocd usage one can check

Using JTAG for imx6 board bringup 

Problems in i.mx6 board with openocd 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

910 Views
wenmingfeng
Contributor III

Thanks igor!

0 Kudos
Reply