JTAG Debugging On SabreLite/Nitrogen6X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG Debugging On SabreLite/Nitrogen6X

Jump to solution
2,326 Views
mlu
Contributor I

What JTAG interface and debug tools are being used successfully with IMX6Q on SabreLite or Nitrogen6X devel boards?

I will be writing a custom U-Boot BSP and would like to have source-level debugging capability.  I tried a Segger J-Link with Segger 20-pin to 9-pin adapter and the latest version of Segger's GDB Server, but GDB does not seem to connect reliably with the IMX6Q on Nitrogen6X.  I also tried Segger's J-Link Commander as a test and I see the following in the GDB Server's log:

Waiting for J-Link connection...
J-Link is connected.
Firmware: J-Link ARM V8 compiled Sep 20 2012 13:27:01
Hardware: V8.00
S/N: 58005844
Checking target voltage...
Listening on TCP/IP port 2331
Connecting to target...WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet = 2)

WARNING: Could not power-up system power domain

Labels (1)
0 Kudos
Reply
1 Solution
1,283 Views
admin
Specialist II

I have been using the Arium LC500S with the Sabrelite board and performed source level debugging.

Arium also has an adapter to go from the standard 20pin cable to the 10pin header on the Sabrelite board.

Regards,

Brett

View solution in original post

0 Kudos
Reply
1 Reply
1,284 Views
admin
Specialist II

I have been using the Arium LC500S with the Sabrelite board and performed source level debugging.

Arium also has an adapter to go from the standard 20pin cable to the 10pin header on the Sabrelite board.

Regards,

Brett

0 Kudos
Reply