JTAG Debugging On SabreLite/Nitrogen6X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG Debugging On SabreLite/Nitrogen6X

ソリューションへジャンプ
2,961件の閲覧回数
mlu
Contributor I

What JTAG interface and debug tools are being used successfully with IMX6Q on SabreLite or Nitrogen6X devel boards?

I will be writing a custom U-Boot BSP and would like to have source-level debugging capability.  I tried a Segger J-Link with Segger 20-pin to 9-pin adapter and the latest version of Segger's GDB Server, but GDB does not seem to connect reliably with the IMX6Q on Nitrogen6X.  I also tried Segger's J-Link Commander as a test and I see the following in the GDB Server's log:

Waiting for J-Link connection...
J-Link is connected.
Firmware: J-Link ARM V8 compiled Sep 20 2012 13:27:01
Hardware: V8.00
S/N: 58005844
Checking target voltage...
Listening on TCP/IP port 2331
Connecting to target...WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet = 2)

WARNING: Could not power-up system power domain

ラベル(1)
0 件の賞賛
返信
1 解決策
1,918件の閲覧回数
admin
Specialist II

I have been using the Arium LC500S with the Sabrelite board and performed source level debugging.

Arium also has an adapter to go from the standard 20pin cable to the 10pin header on the Sabrelite board.

Regards,

Brett

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,919件の閲覧回数
admin
Specialist II

I have been using the Arium LC500S with the Sabrelite board and performed source level debugging.

Arium also has an adapter to go from the standard 20pin cable to the 10pin header on the Sabrelite board.

Regards,

Brett

0 件の賞賛
返信