J1939 support on CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

J1939 support on CAN

2,638 Views
riteshpatel
Contributor II

Hi,

I am working on one project and need J1939 protocol support on CAN interface & I am new to this protocol. I am using iMX6Q processor in my application.

My question is, Which specification I need to check in CAN transceiver to support J1939 protocol on CANbus?

I am planning to use TJA1043 CAN transceiver in my design. Please suggest.

Thanks,

Ritesh

0 Kudos
Reply
2 Replies

2,251 Views
naveenrapheal
Contributor I

Hi Ritesh,

I am not working in the hardware design but I have some experience in J1939 protocol.

SAE J1939 physical layer is coming under ISO 11898.In the data sheet of your TJA1043,it says it will support ISO 11898 (Fully ISO 11898-2:2003 and ISO 11898-5:2007 compliant). So I think this one will work for you.

Thanks

Naveen

0 Kudos
Reply

2,251 Views
riteshpatel
Contributor II

Awaiting for response...!!

0 Kudos
Reply