J1939 support on CAN Transceiver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

J1939 support on CAN Transceiver

5,379 Views
riteshpatel
Contributor II

Hi,

I am working on one project and need J1939 protocol support on CAN interface & I am new to this protocol. I am using iMX6Q processor in my application.

My question is, Which specification I need to check in CAN transceiver to support J1939 protocol on CANbus? 

I am planning to use TJA1043 CAN transceiver in my design. Please suggest.

Thanks, 

Ritesh

0 Kudos
Reply
2 Replies

4,474 Views
naveenrapheal
Contributor I

Hi Ritesh,

 

I am not working in the hardware design but I have some experience in J1939 protocol.

SAE J1939 physical layer is coming under ISO 11898.In the data sheet of your TJA1043,it says it will support ISO 11898(Fully ISO 11898-2:2003 and ISO 11898-5:2007 compliant). So I think this one will work for you.

 

Thanks

Naveen

0 Kudos
Reply

4,474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ritesh

please refer to overview of protocol on

http://www.kvaser.com/external-link/?url=http://www.saedigitallibrary.org/corporate/small-business/j... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply