Issues with android_kk4.4.2_1.0.0-ga on i.MX6Q platform.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issues with android_kk4.4.2_1.0.0-ga on i.MX6Q platform.

跳至解决方案
3,677 次查看
JosephLai
Contributor II

Hello,

 

We're porting android_kk4.4.2_1.0.0-ga bsp to our i.MX6Q board.

 

The MX player halted with ARMv7 NEON H/W+ decoder. (detailed log was attached.)

I/ActivityManager( 2679): START u0 {act=android.intent.action.VIEW dat=file:///storage/emulated/0/Movies/Video/04.mpeg1-Ford 2.mpg cmp=com.mxtech.videoplayer.ad/.ActivityScreen (has extras)} from pid 6797

W/audio_hw_primary( 2300): card 1, port 0 device 0x2

W/audio_hw_primary( 2300): rate 44100, channel 2 period_size 0xc0

V/MX.Player.Screen( 6797): onCreate (com.mxtech.videoplayer.ad.ActivityScreen@41d54cd0) dat=file:///storage/emulated/0/Movies/Video/04.mpeg1-Ford%202.mpg

V/MX.Player.Screen( 6797):     << Extra >>

V/MX.Player.Screen( 6797):  1) from_video_list=true

D/dalvikvm( 6797): GC_CONCURRENT freed 539K, 12% free 4884K/5496K, paused 2ms+6ms, total 26ms

V/MX.Player.Player( 6797): Canonicalizing URI file:///storage/emulated/0/Movies/Video/04.mpeg1-Ford%202.mpg -> file:///storage/emulated/0/Movies/Video/04.mpeg1-Ford%202.mpg

V/MX.Player.Player( 6797): Canonicalizing URI(2) file:///storage/emulated/0/Movies/Video/04.mpeg1-Ford%202.mpg -> file:///storage/emulated/0/Movies/Video/04.mpeg1-Ford%202.mpg

I/MediaFocusControl( 2679):  AudioFocus  requestAudioFocus() from android.media.AudioManager@41b14ac0com.mxtech.videoplayer.ActivityScreen$£½@41d914e0

I/MediaFocusControl( 2679):   Remote Control   registerMediaButtonIntent() for PendingIntent{42141ee0: PendingIntentRecord{422cc558 com.mxtech.videoplayer.ad broadcastIntent}}

E/BufferQueue( 2297): [com.mxtech.videoplayer.ad/com.mxtech.videoplayer.ad.ActivityScreen] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

D/MX.Player.Screen( 6797): === Enter surfaceCreated. holder=android.view.SurfaceView$4@41bd91e8 _surfaceHolderCreated=null_surfaceView=android.view.SurfaceView{41cebe90 V.E..... ......ID 0,0-1366,768 #7f0a0027 app:id/surfaceView}

V/MX.Player.Screen( 6797): HW Accel=true

D/MX.Player.Screen( 6797): === Leave surfaceCreated.

V/MX.Player.Joint( 6797): Creating a joint player. 1st=com.mxtech.media.FFPlayer@41b4f720 2nd=null mix=0

D/MX.Player.Screen( 6797): Set fullscreen = false

I/ActivityManager( 2679): Displayed com.mxtech.videoplayer.ad/.ActivityScreen: +392ms

I/MX      ( 6797): 6863 | Container format='mpeg'

I/OMXClient( 6797): Using client-side OMX mux.

E/MX.Video.Decoder.System( 6797): 6863 | Can't create OMX codec for video/mpeg

F/libc    ( 6797): invalid address or address of corrupt block 0x68a28938 passed to dlfree

F/libc    ( 6797): Fatal signal 11 (SIGSEGV) at 0xdeadbaad (code=1), thread 6863 (.videoplayer.ad)

I/DEBUG   ( 2296): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***

I/DEBUG   ( 2296): Build fingerprint: 'Freescale/sabresd_6dq/sabresd_6dq:4.4.2/1.0.0-rc3/20140630:user/dev-keys'

I/DEBUG   ( 2296): Revision: '405522'

I/DEBUG   ( 2296): pid: 6797, tid: 6863, name: .videoplayer.ad  >>> com.mxtech.videoplayer.ad <<<

I/DEBUG   ( 2296): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad

I/DEBUG   ( 2296): Abort message: 'invalid address or address of corrupt block 0x68a28938 passed to dlfree'

I/DEBUG   ( 2296):     r0 00000000  r1 4014939e  r2 deadbaad  r3 4014cee0

I/DEBUG   ( 2296):     r4 68a28938  r5 40157180  r6 40028000  r7 68a28940

I/DEBUG   ( 2296):     r8 00000001  r9 68dbedf0  sl 6bfa49b0  fp 6a3a13d0

I/DEBUG   ( 2296):     ip 00000001  sp 6bfa4910  lr 4011a7a3  pc 4011a7a4  cpsr 600f0030

I/DEBUG   ( 2296):     d0  0000000000000000  d1  0000000000000000

I/DEBUG   ( 2296):     d2  0000000000000000  d3  0000000000000000

I/DEBUG   ( 2296):     d4  4330000000000001  d5  3ff0000000000000

I/DEBUG   ( 2296):     d6  bc6a626331000000  d7  41781080003347d0

I/DEBUG   ( 2296):     d8  449e0000000004f0  d9  0000000043b91100

I/DEBUG   ( 2296):     d10 0000000000000000  d11 0000000000000000

I/DEBUG   ( 2296):     d12 0000000000000000  d13 0000000000000000

I/DEBUG   ( 2296):     d14 0000000000000000  d15 0000000000000000

I/DEBUG   ( 2296):     d16 685b90d8685b90d8  d17 685b90d8685b90d8

I/DEBUG   ( 2296):     d18 0000000001810804  d19 3ff0000000000000

I/DEBUG   ( 2296):     d20 3fa47ae147ae147b  d21 400ff450e4920c14

I/DEBUG   ( 2296):     d22 4034c1163fefa31e  d23 3ff0000000000000

I/DEBUG   ( 2296):     d24 3fe7325188001433  d25 3fd19b5cefffd79a

I/DEBUG   ( 2296):     d26 0000000000000000  d27 3f895d470d6e9486

I/DEBUG   ( 2296):     d28 3fe797c6a435ce85  d29 3e8f20d95f29baf8

I/DEBUG   ( 2296):     d30 bef375cbdb605373  d31 3fe7bc89cf9e1300

I/DEBUG   ( 2296):     scr 80000013

I/DEBUG   ( 2296):

I/DEBUG   ( 2296): backtrace:

I/DEBUG   ( 2296):     #00  pc 000117a4  /system/lib/libc.so (dlfree+1191)

I/DEBUG   ( 2296):     #01  pc 0000dce3  /system/lib/libc.so (free+10)

I/DEBUG   ( 2296):     #02  pc 00070c3f  /system/lib/libstagefright.so (android::MetaData::~MetaData()+10)

I/DEBUG   ( 2296):     #03  pc 0000d19b  /system/lib/libutils.so (android::RefBase::decStrong(void const*) const+40)

I/DEBUG   ( 2296):     #04  pc 0000a084  /data/app-lib/com.mxtech.videoplayer.ad-1/libmxsysdec.18.so

Original Attachment has been moved to: xmplayer-fail.log.zip

标签 (4)
0 项奖励
回复
1 解答
2,450 次查看
jim_lin
NXP Employee
NXP Employee

Hello Joseph,

regarding MX Player, according to their product FAQ page:

FAQ - MX Player

it leads me to the following page for tech-support:

http://forum.xda-developers.com/apps/mx-player

and found there is similar issue and there is test-build to fix it:

http://forum.xda-developers.com/apps/mx-player/tegra-k1-support-t2809432

could you please take it a try?

Best regards,

Jim.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,450 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Joseph,

It seems that the hosting site of the gapps that you are mentioning is not a official Google server. In this case, you should talk about this issue with your local Freescale FAE, as it may involve Google licenses.

Hope this information will be useful for you. Please accept our apologies for ant inconveniences this may cause. Have a nice day.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,450 次查看
JosephLai
Contributor II

Hi Carlos,

Thanks for your information.

I have reported these issues to Freescale FAE team in Taiwan but still no answer.

How about the MX player issue? It seems not related to google licenses.

0 项奖励
回复
2,450 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Joseph,

Have you ensured that your video file is supported? According with Android kk4.4.2_1.0.0-ga Release Notes, it supports MPEG-PS and MPEG-TS, which typically supports mpeg2 and mpeg4.

You could try with these kinds of video files, or also, try with the default video players (Cactus Player, Gallery).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,450 次查看
JosephLai
Contributor II

Hi Carlos,

Thanks for your answering.

The default Cactus Player can play the file. It also played with default H/W decoder of MX Player. Only H/W+ function not works. (PS. The H/W+ works in android_jb4.2.2_1.1.0-ga BSP.)

0 项奖励
回复
2,451 次查看
jim_lin
NXP Employee
NXP Employee

Hello Joseph,

regarding MX Player, according to their product FAQ page:

FAQ - MX Player

it leads me to the following page for tech-support:

http://forum.xda-developers.com/apps/mx-player

and found there is similar issue and there is test-build to fix it:

http://forum.xda-developers.com/apps/mx-player/tegra-k1-support-t2809432

could you please take it a try?

Best regards,

Jim.

0 项奖励
回复
2,450 次查看
JosephLai
Contributor II

Hi Jim,

Thanks, The test build works.

Best regards,

Joseph.

0 项奖励
回复