Does overlay plan support pixel level transparent (iMX6Q)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does overlay plan support pixel level transparent (iMX6Q)

825 Views
weishanli
Contributor I

Hi

This question is on iMX6Q platfrom, in case of use LCD panel which resolution is 1024x768 on SabreSD board.

  I found a lot of demos on showing camera live view on fb1, but at that case, fb1 works under YUV mode and doesn't support pixel level transparent.

  I'd like to show an icon on fb1 and let it float on main display.

  Would you please tell me if framebuffer fb1, which known as "overlay", support partly transparent or not, if support, how can I change to this mode?

B.R

Weishan

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

628 Views
Yuri
NXP Employee
NXP Employee

  You may try using mfw_isink plugin, described in Appendix A (mfw_isink Usage)

of  "i.MX_6_Series_Yocto_Project_Multimedia_User's_Guide.pdf".

  Also,  please refer to  package with Linux Multimedia Codecs, which contains

Freescale Gstreamer plugins.

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_IMX6QDLS_BUNDLE&appType=license&loc...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply