Issues configuring backlight drivers and initializing PWM output from kernel and user space.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues configuring backlight drivers and initializing PWM output from kernel and user space.

3,074 Views
kevinmahlie
Contributor I

I am having major issues configuring my lcd backlight PWM for the correct configuration. I am using an NXP iMX6 Quad. I have verified that the device tree is correctly configured but I can not even get the PWM to output from the user space control in the terminal window. Also, when I navigate to the back light directory.. cd /sys/class/backlight .....

Has anyone had a similar issues to this or be able to provide any help?

0 Kudos
Reply
1 Reply

2,940 Views
art
NXP Employee
NXP Employee

Please refer to the Chapter 47 of the attached document for the information on how to configure and use the PWM and Backlight driver.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply