The board with WinCE7 support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The board with WinCE7 support.

1,324 Views
glinko13
Contributor I

Hello. We are looking for board, on which we can run WinCE7. We need such features as OpenGL ES support, USB support, and UART support. Our goal is to create multimedia device for automotive. Which board can you suggest?

0 Kudos
Reply
1 Reply

1,249 Views
art
NXP Employee
NXP Employee

NXP by itslef does not provide any support for WinCE7. The support can be achieved through some 3rd party vendors. For example:

https://boundarydevices.com/product/sabre-lite-imx6-sbc/

https://guruce.com/imx6-bsp-releases


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply