Issues about the Same Load on the different Customized Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues about the Same Load on the different Customized Board

1,229 次查看
tony_l_cai
Contributor III

Hi, all

     We have the requirement that we need download the same load,but the custmized board have the different size ddr(no other hw differences),could the freescale Soc support dynamically?

     If support, which Soc,and what we need to do?

3Q~

标签 (6)
0 项奖励
回复
1 回复

1,131 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tony

from hardware (freescale Soc support) point of view

different size ddr is uspported, however existing software does not support

dynamic change, one will have to develop such software.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复