Camera for a MCIMX6Q-SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera for a MCIMX6Q-SDB

1,620 Views
maxschrake
Contributor I

Is it possible to use the camera the Raspberry PI uses for the MCIMX6Q-SDBs camera connector ?

And if not what cameras can i use ?

Greetings Max

0 Kudos
Reply
2 Replies

1,475 Views
SergioSolis
NXP Employee
NXP Employee

If you are referring to this one:

http://www.raspberrypi.org/products/camera-module/

then yes, it is supported, as Saurabh said, you can use the MIPI and CSI interfaces (as well as USB).

You would need to develop your own driver for it though.

0 Kudos
Reply

1,475 Views
saurabh206
Senior Contributor III

Hi Max

IMX6 supports MIPI and CSI camera interface.

0 Kudos
Reply