Issues About Bootargs on MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues About Bootargs on MX6DL

2,109件の閲覧回数
tony_l_cai
Contributor III

Hi all,

        I want to change the baudrate on Android 5.0, and the chipset is MX6DL. now I have changed the uboot 2014 baudrate ,but I cannot change the baudrate in bootargs. and I find whatever modifying or deleting the define of CONFIG_EXTRA_ENV_SETTINGS, the printenv result is as below:

bootargs=console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,if=RGB24,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60 video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled

       I am so confused that I cannot find the params above in the code, so can anybody help me? Thank you~

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,956件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   You may try to change Linux console baudrate :

bootargs=console=ttymxc0,115200

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,956件の閲覧回数
tony_l_cai
Contributor III

Hi Yuri,

Yes,you are right,but I don't know which file can change this param. Could you help me ?

I don't find the file !

0 件の賞賛
返信