Issue when reading tty with nfs rootfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue when reading tty with nfs rootfs

跳至解决方案
1,194 次查看
victorien
Contributor IV

Hi,

For an embedded device (kernel 3.14 and rootfs with OpenEmbedded), I develop a software which read the data on tty driver. This soft operates correctly when I test it on the board. If I use an nfs server for the rootfs the soft is stuck on the loop which read the tty file. I can't go out with 'ctrl+c', I can't write on the console and I have this kind of message " nfs: server 192.168.1.40 not responding, still trying"

Is there someone who knows this issue ?

Thanks

My software :

#include <stdio.h>

#include <stdlib.h>

#include <string.h>

#include <signal.h>

#include <sys/types.h>

#include <sys/stat.h>

#include <fcntl.h>

#include <sys/poll.h>

#include <sys/ioctl.h>

#include <sys/socket.h>

#include <netinet/in.h>

#include <fcntl.h>

#include <termios.h>

#include <sys/fcntl.h>

#include <errno.h>

#include <unistd.h>

#include <time.h>

#define FALSE    0

#define TRUE    1

int print_help (int argc, char *argv[])

{

    printf("Test program for uart reception\n");

    printf("Usage :\n");

    printf("\t%s [-h -D -c]\n", argv[0]);

    printf("\t-D : use this tty device\n");

    printf("\t-c : control data to extract the trame\n");

    printf("\t-h : print help\n");

    return 0;

}

int wait_flag = TRUE ;

void signal_handler_IO (int status)

{

     //printf("received data from UART.\n");

     wait_flag = FALSE;

}

/*

* The values for speed are B115200, B230400, B9600, B19200, B38400, B57600,

* B1200, B2400, B4800, etc. The values for parity are 0 (meaning no parity),*

* PARENB|PARODD (enable parity and use odd), PARENB (enable parity and use even),

* PARENB|PARODD|CMSPAR (mark parity), and PARENB|CMSPAR (space parity).

*/

int set_interface_attribs (int fd, int speed, int parity)

{

    struct sigaction saio;

        struct termios tty;

        memset (&tty, 0, sizeof tty);

     /***/

    saio.sa_handler = signal_handler_IO;

    saio.sa_flags = 0;

    saio.sa_restorer = NULL;

    sigaction(SIGIO, &saio, NULL);

    fcntl (fd, F_SETFL, FNDELAY|FASYNC);

    fcntl (fd, F_SETOWN, getpid());

    /***/

        if (tcgetattr (fd, &tty) != 0)

        {

                printf("error from tcgetattr\n");

                return -1;

        }

        cfsetospeed (&tty, speed);

        cfsetispeed (&tty, speed);

        tty.c_cflag = (tty.c_cflag & ~CSIZE) | CS8;     // 8-bit chars

        // disable IGNBRK for mismatched speed tests; otherwise receive break

        // as \000 chars

        tty.c_iflag &= ~IGNBRK;         // disable break processing

        tty.c_lflag = 0;                // no signaling chars, no echo,

                                        // no canonical processing

        tty.c_oflag = 0;                // no remapping, no delays

        tty.c_cc[VMIN]  = 0;            // read doesn't block

        tty.c_cc[VTIME] = 5;            // 0.5 seconds read timeout

        tty.c_iflag &= ~(IXON | IXOFF | IXANY); // shut off xon/xoff ctrl

        tty.c_cflag |= (CLOCAL | CREAD);// ignore modem controls,

                                        // enable reading

        tty.c_cflag &= ~(PARENB | PARODD);      // shut off parity

        tty.c_cflag |= parity;

        tty.c_cflag &= ~CSTOPB;

        tty.c_cflag &= ~CRTSCTS;

        if (tcsetattr (fd, TCSANOW, &tty) != 0)

        {

                printf("error from tcsetattr\n");

                return -1;

        }

        return 0;

}

/*

* "Blocking" sets whether a read() on the port waits for the specified number

* of characters to arrive. Setting no blocking means that a read() returns

* however many characters are available without waiting for more, up to the

* buffer limit.

*/

void set_blocking (int fd, int should_block)

{

        struct termios tty;

        memset (&tty, 0, sizeof tty);

        if (tcgetattr (fd, &tty) != 0)

        {

                printf ("error from tggetattr\n");

                return;

        }

        tty.c_cc[VMIN]  = should_block ? 1 : 0;

        tty.c_cc[VTIME] = 5;            // 0.5 seconds read timeout

        if (tcsetattr (fd, TCSANOW, &tty) != 0)

                printf ("error setting term attributes\n");

}

int main(int argc, char *argv[]) {

    int i, j, k;

    int fd;

    char c;

    signed char index_trame = -1;

    char trame[6];

    char initChaine[30] = "Frame received on uart :";

    char *ttyDevice = "/dev/ttyAPP0";

    char chaineCar[100];

    char receptCar[6];

    char buf[255];

    char processData[512];

    char restofData[6];

    int sizeofData = 0;

    char ctrl_trame = 0;

    int loop = 0;

    int ret = 0;

    int count = 0;

    FILE* saveFile = NULL;

    /* Parse arguments */

    if (argc < 0 || argc > 4) {

        printf("Invalid number of argument\n");

        print_help(argc, argv);

        return 0;

    }

    j = 0;

    for (i=1; i<argc; i++) {

        if (argv[i][0] == '-') {

            for (k=1; argv[i][k]; k++) {

                switch (argv[i][k]) {

                    case 'D':

                        ttyDevice = argv[i+1];

                        printf("Use %s device\n",ttyDevice);

                        //i++;

                        break;

                    case 'c':

                        ctrl_trame = 1;

                        break;

                    case 'h':

                        print_help(argc, argv);

                        break;

                    default:

                        printf("Wrong option: -%c\n", argv[i][k]);

                        print_help(argc, argv);

                        return 0;

                }

            }

        } else {

        }

        j ++;

    }/**/

    /*run program*/

    printf(" Read serial port V0.6\n");

    saveFile = fopen("receptUart.txt", "w+");

    index_trame = 0;

    /* Ouverture de la liaison serie */

    if ( (fd=open(ttyDevice, O_RDONLY | O_NOCTTY | O_SYNC)) == -1 ) {

        printf("error open %s\n", ttyDevice);

        return -1;

    }

    set_interface_attribs (fd, B2400, 0);

    set_blocking (fd, 1);

    do {

            if (wait_flag == FALSE) {

                ret = read(fd, buf, 255);

                if (ctrl_trame) {

                    for (i=0;i<ret;i++)

                        processData[sizeofData+i] = buf[i];

                    sizeofData += ret;

                    for (i=0;i<sizeofData;i++) {

                        if ((sizeofData - i) < 6) {

                            break;

                        }

                        else if (processData[i] == 0xfa) {

                            count++;

                            printf ("Received frame n %d :", count);

                            for (j=0;j<6;j++) {

                                trame[j]=processData[i];

                                printf(" h%02x", processData[i]);

                                i++;

                            }

                            i--;

                            printf("\n");

                        }

                    }

                    for(j=i;j<sizeofData;j++)

                        processData[j-i] = processData[j];

                    sizeofData -= i;

                }

                else {

                    printf ("%i data received :", ret);

                    for (i=0;i<ret;i++) {

                        printf(" h%02x", buf[i]);

                    }

                    printf("\n");

                }

                wait_flag = TRUE;

            }

    }

    while (1);

    close(fd);

    printf("GoodBye\n");

    return EXIT_SUCCESS;

}

标签 (2)
0 项奖励
回复
1 解答
1,070 次查看
victorien
Contributor IV

I found the problem : it's a bad setting on devicetree.

UART 0 port was setting to use CTS/RTS line and the ethernet PHY is connected to CTS/RTS pin for control (default setting on evaluation board). Then this pin was used for 2 drivers and one of them crash.

I change UART setting to doesn't use CTS/RTS and it's works

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,071 次查看
victorien
Contributor IV

I found the problem : it's a bad setting on devicetree.

UART 0 port was setting to use CTS/RTS line and the ethernet PHY is connected to CTS/RTS pin for control (default setting on evaluation board). Then this pin was used for 2 drivers and one of them crash.

I change UART setting to doesn't use CTS/RTS and it's works

0 项奖励
回复